SPRADB3 October 2023 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM263P4 , AM263P4-Q1
Table 4-1 contains a comprehensive list of Errata items from AM263 and outlines in which issues are fixed in either Rev 1.1 of AM263 or Rev 1.0 of AM263P. Full details for the errata items are provided in AM263x Sitara™ Microcontroller Silicon Revision 1.0A, 1.1.
Module | Description | Silicon Revisions Affected | ||
---|---|---|---|---|
AM263x | AM263P | |||
1.0A | 1.1 | 1.0 | ||
CLOCKS | i2324 — No synchronizer present between GCM and GCD status signals | Present | Present | Present |
QSPI | i2364 — QSPI: Access to address beyond 8MB is not supported in mem map mode | Present | Present | New OSPI module can support addresses beyond 8MB |
VDDA | i2348 — VDDA1V8 Static Power leakage | Present | Fixed | Fixed |
ADC | i2346 — ADC result has Error when switching between odd and even channels | Present | Fixed | Fixed |
ADC | i2347 — VREF current consumption of ADC is random at powerup | Present | Fixed | Fixed |
ADC | i2349 — ADC VrefHi Loading increase in powerdown | Present | Fixed | Fixed |
CONTROLSS | i2352 — CONTROLSS-SDFM: Dynamically Changing Threshold Settings (LLT, HLT), Filter Type, or COSR Settings Will Trigger Spurious Comparator Events | Present | Present | Present |
CONTROLSS | i2353 — CONTROLSS-SDFM: Dynamically Changing Data Filter Settings (Such as Filter Type or DOSR) Will Trigger Spurious Data Acknowledge Events | Present | Present | Present |
CONTROLSS | i2354 — CONTROLSS-SDFM: Two Back-to-Back Writes to SDCPARMx Register Bit Fields CEVT1SEL, CEVT2SEL, and HZEN Within Three SD-Modulator Clock Cycles can Corrupt SDFM State Machine, Resulting in Spurious Comparator Events | Present | Present | Present |
CONTROLSS | i2355 — CONTROLSS-ADC: DMA Read of Stale Result | Present | Present | Fixed |
CONTROLSS | i2356 — CONTROLSS-ADC: Interrupts may Stop if INTxCONT (Continue-to-Interrupt Mode) is not Set | Present | Present | Present |
CONTROLSS | i2357 — CONTROLSS-ePWM: An ePWM Glitch can Occur if a Trip Remains Active at the End of the Blanking Window | Present | Present | Present |
CONTROLSS | i2358 — CONTROLSS-ePWM: Trip Events Will Not be Filtered by the Blanking Window for the First 3 Cycles After the Start of a Blanking | Present | Present | Present |
CONTROLSS | i2359 — CONTROLSS-CMPSS:Prescaler counter behaviour different from spec when DACSOURCE is made 0 or reconfigured as 1 | Present | Present | Present |
CONTROLSS | i2405 — Race condition OUTPUT_XBAR and PWM_XBAR resulting in event miss | Present | Present | Present |
CPSW | i2345 — CPSW: Ethernet Packet corruption occurs if CPDMA fetches a packet which spans across memory banks | Present | Present | Present |
CPSW | i2401 — Host Timestamps Cause CPSW Port to Lock up | Present | Present | Present |
CPSW | i2402 — Ethernet to Host Checksum Offload does not work | Present | Present | Fixed |
CPSW | i2329 — MDIO interface corruption (CPSW and PRU-ICSS) | Present | Fixed | Fixed |
CRC | i2386 — CRC 8-bit data width and CRC8-SAE-J1850 and CRC8-H2F possible use in CAN module is not supported | Present | Present | Fixed |
DCC | i2395 — DCC Module Frequency Comparison can Report Erroneous Results | Present | Present | Fixed |
GPMC | i2313 — GPMC: Sub-32-bit read issue with NAND and FPGA/FIFO | Present | Present | Not Applicable |
M4 ROM | i2403 — SBL redundant boot image feature not supported on HSSE devices | Not Applicable | Present | Not Applicable |
MBOX | i2404 — Race condition in mailbox registers resulting in events miss | Present | Present | Present |
McSPI | i2350 — McSPI data transfer using EDMA in ‘ABSYNC’ mode stops after 32 bits transfer | Present | Present | Fixed |
MSS_CTRL | i2392 — Race condition in mem-init capture registers resulting in events miss | Present | Present | Present |
MSS_CTRL | i2394 — Race condition in interrupt and error aggregator capture registers resulting in events miss | Present | Present | Present |
R5FSS | i2374 — PBIST fails if clock frequency of R5SS_CORE_CLK is not same as R5FSS_CLK_SELECTED frequency | Present | Present | Present |
SDFM | i2375 — SDFM module event flags (SDIFLG.FLTx_FLG_CEVTx) do not get set again if the comparator event is still active and digital filter path (using SDCOMPxCTL.CEVTxDIGFILTSEL) is being selected | Present | Present | Fixed |
UART | i2310 — USART: Erroneous triggering of timeout interrupt | Present | Present | Present |
UART | i2311 — USART: Spurious DMA Interrupts | Present | Present | Present |