To run this lab, make sure the
hardware is set up as outlined in the previous section,Section 3.4.2.
Open the CCS project as outlined
in Section 3.2.1. If
using the powerSUITE, go to Step 3, otherwise jump to Step 4.
Open the SYSCONFIG page and
select under the Build Options section:
Select Lab 2: Closed
Loop CC Single Phase for the Lab.
Change the Phase
Enabled to Phase 1 or Phase 2>
Set the SFRA
Enable/Disable to 1.
Open the Compensation
Designer by clicking the Run Compensation
Design button.
The compensation designer
then launches and prompts the user to select a valid SFRA data file.
Import the SFRA data from the run in Lab 1 into the compensation
designer to design a two-pole, two-zero compensator. Keep more margins
during this iteration of the design to make sure that when the loop is
closed, the system is stable.
Figure 3-24 shows compensation parameters for the Current Loop.
Click on the Save
Comp button to save the compensation. Close the Compensation
Designer tool.
Save the SYSCONFIG
page.
When using non-powerSuite version
of the project, Build Settings are directly modified in
solution_settings.h file. Compensation Designer is found at
C2000Ware_DigitalPower_Install_Location\powerSUITE\source\utils.
#define LAB_NUMBER
(2)
#define PHASE_NUMBER (1)
#define SFRA_ENABLED
(true)
Figure 3-16 Tuning Current Loop Using
Compensation Designer