Use the following steps to build and load the
project and to set up the debug environment.
- Right-click on the project name and click
Rebuild Project.
- The project builds successfully.
- In the Project Explorer, make sure the correct
target configuration file is set as Active under targetConfigs.
- Then, click Run → Debug to launch a
debugging session.
- The project then loads on the device and the CCS
debug view becomes active. The code halts at the start of the main routine.
- To add the variables in the watch/expressions
window, click View → Scripting Console to open the scripting
console dialog box. On the upper right corner of this console, click on
open and then browse to the setupdebugenv_lab1_ch1.js script
file located inside the project folder. This populates the watch window with the
appropriate variables needed to debug the system. For phase 2, select
setupdebugenv_lab2_ch2.js script file.
- Click on the Continuous Refresh button
on the watch window to enable continuous update of
values from the controller.