TIDUF35 june 2023 AM6442
The AM6442 SoC UART0 interface is used to interface the PC with the Linux serial terminal console. The AM6442 UART0 port is interfaced with FT232RQ for UART-to-USB functionality and terminated on a micro B connector (J12). When the EVM is connected to a PC host using the provided USB cable, the PC host can establish a Virtual Com Port which can be used with any terminal emulation application. The FT332RQ is bus powered. Virtual Com Port drivers for the FT232RQ can be obtained from manufacturers website: ftdichip.com/products/ft232rq/.