SLVSIL6C January 2026 – April 2026 INA151
PRODUCTION DATA
The topology in the INA151 build in an input bias current stage that requires a typical common-mode bias current of 20μA to allow operate at very high common-mode voltages. As shown in Figure 7-4, the bias stage allows the common-mode bias current to be constant across the common-mode range, enabling minimal error implications for a precision voltage monitoring system.
The bias circuit in the INA151 includes resistance between the input pins with an effective differential input impedance of 45kΩ. This differential impedance creates differential input bias current flowing in and out of the device proportional to the input differential voltage, depicted in Figure 7-5. The total input bias current for each input pin is the summation of the common-mode leakage from input to reference, IBCM, and the differential current, IBDIFF.