SNVSA47D February 2016 – December 2022 LM5165
PRODUCTION DATA
Tie RT to GND to select PFM mode of operation. The inductor, input voltage, output voltage, and peak current determine the pulse switching frequency of a PFM-configured LM5165. For a given input voltage, output voltage and peak current, the inductance of LF sets the switching frequency when the output is in regulation. Use Equation 19 to select an inductance of 47 µH based on the target PFM converter switching frequency of 350 kHz at 12-V input.

IPK(PFM) in this example is the peak current limit setting of 120 mA plus an additional 10% margin added to include the effect of the 100-ns peak current comparator delay. An additional constraint on the inductance is the 180-ns minimum on-time of the high-side MOSFET. Therefore, to keep the inductor current well controlled, choose an inductance that is larger than LF(min) using Equation 20 where VIN(max) is the maximum input supply voltage for the application, tON(min) is 180 ns, and IL(max) is the maximum allowed peak inductor current.

Choose an inductor with saturation current rating above the peak current limit setting, and allow for derating of the saturation current at the highest expected operating temperature.