SNOSDA2E august 2020 – july 2023 TLV3604 , TLV3605 , TLV3607
PRODMIX
Since input bias is typically 1 µA, it is best to choose a value for R1 and then solve for the required R2 to provided the needed amount of hysteresis. In this example, a value of 500 Ω was selected to minimize the impact of input bias current on circuit offset voltage. Solving for R2 provides the equation below. Note that VOD is 350 mV from the EC Table.
VREF can now be solved for using the equation for VINN_LOW or VINN_HI. IN this example, VINN_HI was chosen.
The external hysteresis design is now complete with R1 = 500 Ω, R2 = 8.25 kΩ, VREF = 2.8 V.