SLVSI74A July 2025 – November 2025 TLV61290
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
The TLV61290 device features an average inductor current limit scheme.
In dc/dc boost mode, the TLV61290 device employs a current limit detection scheme in which the voltage drop across the synchronous rectifier is sensed during the off-time. The average current limit threshold is set via an I2C register. The default average current limit in boost mode is approximately 8A, when it hits the current limit, the device works in constant current mode. The output voltage is reduced as the power stage of the device operates in a constant current mode.
The output voltage is reduced as the power stage of the device operates in a constant current mode. The maximum continuous output current (IOUT(max)), before entering current limit (CL) operation, is defined by Equation 6.
where
The output current, IOUT, is the average of the rectifier ripple current waveform. When the load current is increased such that the trough is above the current limit threshold, the off-time is increased to allow the current to decrease this threshold before the next on-time begins (so called frequency fold-back mechanism). When the current limit is reached the output voltage decreases during further load increase.
In true bypass mode, the TLV61290 device employs a hiccup protection scheme. The current limit threshold is set using an I2C register. The default current limit in true bypass mode is 10A, when it hits the current limit, the device turns off the bypass FET after a small delay, ca. 200ns, then the device enters into hiccup mode. Once the short-circuit is released, the TLV61290 goes through the soft start-up again.