SBOSA71 July 2021 TMCS1107-Q1
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
Nonlinearity is the deviation of the output voltage from a linear relationship to the input current. Nonlinearity voltage, as shown in Figure 8-1, is the maximum voltage deviation from the best-fit line based on measured parameters, calculated by Equation 7.
where
Nonlinearity error (eNL) for the TMCS1107-Q1 is the nonlinearity voltage specified as a percentage of the full-scale output range (VFS), as shown in Equation 8.