SBOSAF4A January 2025 – June 2025 TMCS1123-Q1
PRODUCTION DATA
The ideal first-order transfer function of the TMCS1123-Q1 is given by Equation 1, where the output voltage is a linear function of input current. The accuracy of the device is quantified both by the error terms in the transfer function parameters, as well as by nonidealities that introduce additional error terms not in the simplified linear model. See Total Error Calculation Examples for example calculations of total error, including all device error terms.
where