SBOSA50A December 2021 – March 2022 TMP127-Q1
PRODUCTION DATA
The TMP127-Q1 will convert temperature at a 200-ms interval with a maximum conversion period of 270 ms per the Section 7.5 table. Reading from the TMP127-Q1 faster than the conversion period can result in data being retrieved twice before new data is available. Therefore TI recommends to read from the TMP127-Q1 in intervals greater than the maximum conversion period (like every 300 ms, for example). Reading faster than the conversion period will not disrupt device operation and can safely be done if desired.
In the read-only configuration, the TMP127-Q1 is not connected to a controller PICO pin. Due to this if the SCLK pin were to continue to be clocked for the write portion of the transaction, the SIO pin would be floating and the write value undetermined. It is for this reason that TI recommends to only perform the first 16 clock cycles to read the TMP127-Q1 temperature date and pull CS high after, as shown in Figure 9-1. This will ensure the TMP127-Q1 is never written to with a floating input.