SPRS945G January 2017 – January 2023 TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1
PRODUCTION DATA
Figure 10-2 and Figure 10-3 provide examples of the F28004x device markings and define each of the markings. The device revision can be determined by the symbols marked on the top of the package as shown in Figure 10-2. Some prototype devices may have markings different from those illustrated.
Figure 10-2 Examples of Device Markings for PM and PZ Packages
Figure 10-3 Example of Device Markings for RSH Package| SILICON REVISION CODE | SILICON REVISION | REVID(1) Address: 0x5D00C | COMMENTS |
|---|---|---|---|
| Blank | 0 | 0x0000 0000 | This silicon revision is available as TMX. |
| A | A | 0x0000 0001 | This silicon revision is available as TMX. |
| B | B | 0x0000 0002 | This silicon revision is available as TMX and TMS. |