SLVSHM3 November 2026 TPS2HCS05-Q1
PRODUCTION DATA
For TPS2HCS05B-Q1, the AUTO_LPM_EXIT_CH bit has no effect on the TPS2HCS05B-Q1. The system can manually transition the TPS2HCS05B-Q1 device out of AUTO_LPM by changing the state of the DI pin in AUTO_LPM state.
For TPS2HCS05A-Q1, the MCU or controller can write a 1 to the either or both AUTO_LPM_EXIT_CHx bits to manually transition the device out of the AUTO_LPM state to the ACTIVE state. If either AUTO_LPM_EXIT_CHx are 1 then the corresponding channel is enabled if not already enabled when the device is in ACTIVE state. For TPS2HCS05A-Q1, both AUTO_LPM_EXIT_CHx bits have to be set back to 0 before the device is allowed to transition back to the AUTO_LPM state.
For TPS2HCS05B-Q1, the AUTO_LPM_EXIT_CHx bits have no effect on the TPS2HCS05B-Q1. The system can manually transition the TPS2HCS05B-Q1 device out of AUTO_LPM by changing the state of DI1 or DI2 or both in AUTO_LPM state.