SLVSHM3 November 2026 TPS2HCS05-Q1
PRODUCTION DATA
The AUTO_LPM state provides a mode where the device can automatically transition to a low IQ state while keeping the channels on, if desired, and protected through short-circuit protection. Depending on the device version used, to enter the AUTO_LPM state the AUTO_LPM_ENTRY bit in the DEV_CONFIG register must be set to 1 and the following conditions need to be met for at least tSTBY_LPM_AUTO:
Once the conditions are met, the device updates the LPM_STATUS bit in the SDO frame/GLOBAL_FAULT_TYPE register and the LPM_STATUS_1 bit in the GLOBAL_FAULT_TYPE register before entering the AUTO_LPM state to alert the system that device has transitioned to AUTO_LPM. The device enters AUTO_LPM state in tLPM_ENTRY.
Note: If the device is configured to the MANUAL_LPM state before setting the AUTO_LPM_ENTRY bit to 1, additional SPI commands are required to enable Auto LPM Entry. To specify a safe transition from Manual LPM to Auto LPM, if the device exits Manual LPM due to a Load Step or Short Circuit event, the MANUAL_LPM bit must be set to 1 and then reset to 0. After this entry and exit from the Manual LPM state is complete, the AUTO_LPM_ENTRY bit can be set to 1, and the device enters Auto LPM once all conditions are met.
In the AUTO_LPM state, the larger internal FET is used to allow for larger load steps. The RON for the larger internal FET is defined by the RON,LPM_AUTO in the electrical characteristics section. The IQ in AUTO_LPM is higher compared to the small FET operation in MANUAL_LPM state and roughly the same as the MANUAL_LPM state with the larger FET operation. In AUTO_LPM, the entry threshold is specified by IENTRY_LPM_AUTO and the exit threshold is specified by IEXIT_LPM_AUTO.