SBVS065L December 2005 – December 2024 TPS74301
PRODUCTION DATA
The device can have VIN, VBIAS, VEN, and VTRACK sequenced in any order without causing damage to the device. However, for the track function to work as intended, certain sequencing rules must be applied. VBIAS must be present and the device enabled before the track signal starts to ramp. VIN must ramp up faster than the external supply being tracked so that the tracking signal does not drive the device into VIN dropout as VOUT ramps up. The preferred method to sequence the tracking device is to have VIN, VBIAS, and VEN above the minimum required voltages before enabling the master supply to initiate the startup sequence. This method is illustrated in Figure 7-3. Resistors R3 and R4 disable the master supply until the input voltage is above 3.52V (typical).
If the TRACK pin is not needed the pin must be connected to VIN for the legacy chip, for the new chip this pin can be left floating. Configured in this way, the device starts up typically within 40μs (legacy chip) or 100µs (new chip), which can result in large inrush current that can cause the input supply to droop. If soft-start is needed, consider the TPS742 or TPS744 devices.