SBVS397A September 2023 – November 2023 TPS7B4256-Q1
PRODUCTION DATA
A feedforward capacitor (CFF) is recommended to be connected between the OUT pin and the FB pin. CFF improves transient, noise, and PSRR performance. A higher capacitance CFF can be used; however, the start-up time increases. For a detailed description of CFF tradeoffs, see the Pros and Cons of Using a Feedforward Capacitor with a Low-Dropout Regulator application note.
As shown in Figure 7-2, poor layout practices and using long traces at the FB pin results in the formation of a parasitic capacitor (CFB).
CFB, along with the feedback resistors R1 and R2 can result in the formation of an uncompensated pole in the transfer function of the loop gain. A CFB value as small as 7 pF can cause the parasitic pole frequency, given by Equation 7, to fall within the bandwidth of the LDO and result in instability.
Adding a feedforward capacitor (CFF), as shown in Figure 7-3, creates a zero in the loop gain transfer function that can compensate for the parasitic pole created by CFB. Equation 8 and Equation 9 calculate the pole and zero frequencies.
The CFF value that makes fP equal to fZ, and result in a pole-zero cancellation, depends on the values of CFB and the feedback resistors used in the application. Alternatively, if the feedforward capacitor is selected so that CFF ≫ CFB, then the pole and zero frequencies given by Equation 8 and Equation 9 are related as:
In most applications, particularly where a 3.3-V or 5-V VOUT is generated, this ratio is not very large, implying that the frequencies are located close to each other and therefore the parasitic pole is compensated. Even for large VOUT values, where this ratio can be as large as 20, a CFF value in the range 100 pF ≤ CFF ≤ 10 nF typically helps prevent instability caused by the parasitic capacitance on the feedback node.
Following good layout practices, as described in the Layout Guidelines section and in the TRKRLDOEVM-119 General-Purpose Tracker LDO Evaluation Module user guide, helps minimize the parasitic feedback pin capacitance to values that prevent the resulting parasitic pole from causing instability.