JAJSPL3 January 2023 BQ21080
PRODUCTION DATA
To obtain optimal performance, the decoupling capacitor from IN to GND, the capacitor from SYS to GND and BAT to GND should be placed as close as possible to the device, with short trace runs to IN, SYS, BAT and GND.Have solid ground plane that is tied to the GND bump
The pushbutton GND should be connected close to the device as possible.
The high current charge paths into IN, SYS and BAT pins must be sized appropriately for the maximum charge current in order to avoid voltage drops in these traces.