The THS403x are available in a thermally-enhanced DGN package, which is a
member of the PowerPAD™ integrated circuit
package family. This package is constructed using a downset lead frame upon which
the die is mounted [see Figure 7-9(a) and Figure 7-9(b)]. This arrangement results in the lead frame exposed as a thermal pad on the
underside of the package [see Figure 7-9(c)]. Because this thermal pad has direct thermal contact with the die, excellent
thermal performance can be achieved by providing a good thermal path away from the
thermal pad.
The PowerPAD integrated circuit
package allows for both assembly and thermal management in one manufacturing
operation. During the surface-mount solder operation (when the leads are soldered),
the thermal pad can be soldered to a copper area under the package. By using thermal
paths within this copper area, heat is conducted away from the package into a ground
plane or other heat-dissipating device.
The PowerPAD integrated circuit
package represents a breakthrough in combining the small area and ease of assembly
of surface mount with the more-recent, awkward mechanical methods of sinking
heat.
Although there are many ways to
properly dissipate heat from this device, the following steps show the recommended
approach.
- Prepare the PCB with a top-side
etch pattern as shown in Figure 7-10. There must be etch for the leads as well as etch for the thermal pad.
- Place five holes in the area of
the thermal pad. These holes must be 13 mils (0.3302 mm) in diameter. The reason
to keep the holes small is to discourage solder wicking through the holes during
reflow.
- Additional vias can be placed
anywhere along the thermal plane outside of the thermal pad area. This action
helps dissipate the heat generated by the THS403x device. The additional vias can be of any diameter because
wicking is not a concern outside of the thermal pad area.
- Connect all holes to the internal
ground plane.
- When connecting these holes to
the ground plane, do not use the typical web or spoke via connection
methodology. Web connections have a high thermal-resistance connection that is
useful for slowing the heat transfer during soldering operations. This makes the
soldering of vias that have plane connections easier. In this application,
however, low thermal resistance is desired for the most efficient heat transfer.
Therefore, the holes under the THS403x
package must connect to the internal ground plane with a complete connection
around the entire circumference of the plated-through hole.
- The top-side solder mask must
leave the pins of the package and the thermal pad area with the five holes
exposed. The bottom-side solder mask must cover the five holes of the thermal
pad area, which prevents solder from pulling away from the thermal pad area
during the reflow process.
- Apply solder paste to the exposed
thermal pad area and to all the device pins.
- With these preparatory steps in
place, the THS403x device is placed in
position and run through the solder reflow operation as any standard
surface-mount component.