JAJSSS6 January 2024 TPS7H3014-SP
ADVANCE INFORMATION
The FAULT pin is an open-drain output that the user can use to monitor if an internal fault has been induced by the state machine. Is recommended to pull this pin to the VLDO output via a 10kΩ resistor. Another voltage source can be used if needed, but is important that this voltage is stable and greater than 1V at all times. The maximum voltage at this pin is 7V. For proper operation this voltage must be stable before attempting a sequence up/down and must never go below 1V during the device operation. The open-drain FET is forced low when the internal state machine of the sequencer detects a fault as described in State Machine .