JAJSKM1C october 2019 – september 2021 UCC5870-Q1
PRODUCTION DATA
Edge Mode (CFG7[ADC_SAMP_MODE] = 0b01) begins the ADC conversions based on the INP edge. When INP transitions, the ADC begins conversions for the round robin after the programmable delay time (programmed using CFG7[ADC_SAMP_DLY]). The channels selected for the PWM ON time are sampled after a rising edge of INP, while the channels selected for the PWM OFF time are sampled after a falling edge. The round robin continues until the next edge of INP. The timing for Edge mode is illustrated in the following figures.
Figure 7-6 ADC edge sampling mode
Figure 7-7 ADC Edge sampling mode timing chart