JAJSKM1C october 2019 – september 2021 UCC5870-Q1
PRODUCTION DATA
When using Center sampling mode (CFG7[ADC_SAMP_MODE]=0b00), the center is calculated for the ON or OFF time on INP (depending on the channel selection setup) based on the previous switching cycle. One channel is sampled during each ON or OFF time depending on the channel selections. The timing for Center mode is illustrated in the following figures.
Figure 7-4 ADC center sampling mode
Figure 7-5 ADC center sample mode timing chart