SBAA535A March 2022 – March 2024 ADC128D818 , ADS1000 , ADS1000-Q1 , ADS1013 , ADS1013-Q1 , ADS1014 , ADS1014-Q1 , ADS1015 , ADS1015-Q1 , ADS1018 , ADS1018-Q1 , ADS1100 , ADS1110 , ADS1112 , ADS1113 , ADS1113-Q1 , ADS1114 , ADS1114-Q1 , ADS1115 , ADS1115-Q1 , ADS1118 , ADS1118-Q1 , ADS1119 , ADS1120 , ADS1120-Q1 , ADS112C04 , ADS112U04 , ADS1130 , ADS1131 , ADS1146 , ADS1147 , ADS1148 , ADS1148-Q1 , ADS114S06 , ADS114S06B , ADS114S08 , ADS114S08B , ADS1158 , ADS1216 , ADS1217 , ADS1218 , ADS1219 , ADS1220 , ADS122C04 , ADS122U04 , ADS1230 , ADS1231 , ADS1232 , ADS1234 , ADS1235 , ADS1235-Q1 , ADS1243-HT , ADS1246 , ADS1247 , ADS1248 , ADS124S06 , ADS124S08 , ADS1250 , ADS1251 , ADS1252 , ADS1253 , ADS1254 , ADS1255 , ADS1256 , ADS1257 , ADS1258 , ADS1258-EP , ADS1259 , ADS1259-Q1 , ADS125H01 , ADS125H02 , ADS1260 , ADS1260-Q1 , ADS1261 , ADS1261-Q1 , ADS1262 , ADS1263 , ADS127L01 , ADS1281 , ADS1282 , ADS1282-SP , ADS1283 , ADS1284 , ADS1287 , ADS1291 , LMP90080-Q1 , LMP90100 , TLA2021 , TLA2022 , TLA2024
Table 8-8 reports the system parameters that determine the cycle time in Example #2:
| PARAMETER | VALUE |
|---|---|
| ADC | ADS124S08 |
| ODR | 1000 SPS |
| Filter type | sinc3 |
| Clock frequency | 4.096 MHz (default) |
| Conversion mode | Single-shot |
| Programmable delay | 14 ∙ tMOD (default) |
| Chopping | Disabled |
| Conversions per channel | 3 |
| # of channels | 2 |
The only difference between Example #1 and Example #2 is that Example #2 now uses single-shot conversion mode. This choice means that all three conversion results on each channel are subject to first conversion latency.
Reviewing Table 5-1, the ADS124S08 first conversion latency using the sinc3 filter and ODR = 1000 SPS is 3.156 ms for first conversion data (tFC). This time assumes that the default clock frequency, fCLK, of 4.096 MHz is used, which is the case for this example. Also, this time includes the ADC overhead but does not include the programmable delay, tDELAY. Equation 10 calculates the value of tDELAY in microseconds using the default value of tDELAY = 14 ∙ tMOD and fCLK = 4.096 MHz:
The ADS124S08 programmable delay applies to each conversion using single-shot mode, resulting in a first conversion latency including programmable delay, tFC_TOTAL, as per Equation 11:
Finally, there is no need to consider additional latency due to chopping. Equation 13 calculates the cycle time, tCYCLE, using the scan time for one channel, tCH, that results from Equation 12. This assumes that the user starts the next conversion on each channel immediately after the previous conversion result is ready:
Ultimately, the cycle time for this example is 19.266 ms for 6 conversion results. Figure 8-2 depicts a timing diagram for the example system given the design parameters.