SBAU249A October   2015  – July 2025 ADS9110

 

  1.   1
  2.   2
  3.   Trademarks
  4. 1Evaluation Module Overview
    1. 1.1 ADS9110EVM-PDK Features
    2. 1.2 ADS9110EVM Features
  5. 2Analog Interface
    1. 2.1 Connectors for Differential Signal Source
    2. 2.2 ADC Differential Input Signal Driver
      1. 2.2.1 Input Signal Path
      2. 2.2.2 Input Common-Mode Jumper Configuration
      3. 2.2.3 R1 Setting vs Source Impedance
    3. 2.3 Onboard ADC Reference
  6. 3Digital Interfaces
    1. 3.1 multiSPI® for ADC Digital IO
  7. 4Power Supplies
  8. 5 ADS9110EVM-PDK Initial Setup
    1. 5.1 Default Jumper Settings
    2. 5.2 EVM Graphical User Interface (GUI) Software Installation
  9. 6 ADS9110EVM-PDK Operation
    1. 6.1 EVM GUI Global Settings for ADC Control
    2. 6.2 Register Map Configuration Tool
    3. 6.3 Time Domain Display Tool
    4. 6.4 Spectral Analysis Tool
    5. 6.5 Histogram Tool
    6. 6.6 Linearity Analysis Tool
  10. 7Hardware Design Files
    1. 7.1 Schematics
    2. 7.2 PCB Layout
    3. 7.3 Bill of Materials
  11. 8Revision History

EVM Graphical User Interface (GUI) Software Installation

Download the latest version of the EVM GUI installer from the Tools and Software folder of the ADS9110 and run the GUI installer to install the EVM GUI software on the user’s computer.

CAUTION: Manually disable any antivirus software running on the computer before downloading the EVM GUI installer onto the local hard disk. Otherwise, depending on the antivirus settings, an error message can appear or the installer.exe file can be deleted.

Accept the license agreements and follow the on-screen instructions to complete the installation.

 ADS9110 Software Installation PromptsFigure 5-1 ADS9110 Software Installation Prompts

As a part of the ADS9110EVM GUI installation, a prompt with a Device Driver Installation appears on the screen. Click Next to proceed.

 Device Driver Installation Wizard PromptsFigure 5-2 Device Driver Installation Wizard Prompts
Note:

A notice can appear on the screen stating that Widows cannot verify the publisher of this driver software. Select Install this driver software anyway.

The ADS9110EVM-PDK requires LabVIEW™ Run-Time Engine and can prompt for the installation of this software, if not already installed.

 LabVIEW Run-Time Engine InstallationFigure 5-3 LabVIEW Run-Time Engine Installation

After these installations, verify that C:\Program Files (x86)\Texas Instruments\ADS9110EVM is as shown in Figure 5-4.

 ADS9110EVM-PDKFolder Post-Installation Figure 5-4 ADS9110EVM-PDKFolder Post-Installation