SBAU251B July 2017 – February 2023 ADS8331 , ADS8332
The following steps list the directions to install the software.
Manually disable any antivirus software running on the computer before downloading the EVM GUI installer onto the local hard disk. Otherwise, depending on the antivirus settings, an error message may appear or the installer.exe file may be deleted.
Download the latest version of the EVM GUI installer from the Tools and Software folder of the ADS8332EVMV2-PDK, and run the GUI installer to install the EVM GUI software. Administrator privileges on the PC are required in order to install the EVM software. Accept the license agreements and follow the on-screen instructions shown in Figure 5-2 in order to complete the installation.
Figure 5-2 Software Installation PromptsAs a part of the ADS8332EVMV2 GUI installation, a prompt with a Device Driver Installation appears on the screen, as shown in Figure 5-3. Click Next to proceed.
Figure 5-3 ADS8332 Device Driver Installation Wizard PromptsA notice may appear on the screen stating that Widows cannot verify the publisher of this driver software. Select Install this driver software anyway.
The ADS8332EVMV2-PDK requires LabVIEW™ Run-Time Engine, and may prompt for the installation of this software, as shown in Figure 5-4, if not already installed.
Figure 5-4 LabVIEW Run-Time Engine InstallationAfter these installations, verify that C:\Program Files (x86)\Texas Instruments\ADS8332EVM is as shown in Figure 5-5.
Figure 5-5 ADS8332EVM Folder Post-Installation