SBAU416C November 2022 – March 2025 ADS9813 , ADS9817
After the EVM GUI is started, press the following buttons in the order shown below. After selecting the desired ADC from the drop-down menu, click BOARD STARTUP. After the USB Status, FPGA Power, and FPGA Program lights are green, click INITIALIZE DEVICE.
The block diagram figures can be used to configure certain settings of the device. The "Device Registers" Tab may be used for more comprehensive device configuration. Press REFRESH on the block diagram to reflect updated device register settings.