SLAA890A December 2019 – August 2021 MSP430FR2000 , MSP430FR2032 , MSP430FR2033 , MSP430FR2100 , MSP430FR2110 , MSP430FR2111 , MSP430FR2153 , MSP430FR2155 , MSP430FR2310 , MSP430FR2311 , MSP430FR2353 , MSP430FR2355 , MSP430FR2422 , MSP430FR2433 , MSP430FR2475 , MSP430FR2476 , MSP430FR2512 , MSP430FR2522 , MSP430FR2532 , MSP430FR2533 , MSP430FR2632 , MSP430FR2633 , MSP430FR2672 , MSP430FR2673 , MSP430FR2675 , MSP430FR2676 , MSP430FR4131 , MSP430FR4132 , MSP430FR4133
Each application is unique and has different reference voltage considerations. As an example, when connecting a sensor to the ADC front-end, you would need to consider the voltage dynamic range, the sensor settling time, powering and disabling the sensor when needed for an energy optimized application. After these considerations are understood, the ADC reference can be tailored for various applications through the configuration registers. Consideration areas for the reference voltage are described in the following sections.