SLAU723A October 2017 ā October 2018 MSP432E401Y , MSP432E411Y
Operations such as data-write, password set, protection set, and copy buffer erase can perform multiple operations. For example, a normal write performs two underlying writes: the control word write and the data write. If the control word writes but the data fails (for example, due to a voltage drop), the overall write fails with indication provided in the EEDONE register. Failure and the corrective action is broken down by the type of operation:
After a reset and prior to writing any data to the EEPROM, software must read the EESUPP register and check for the presence of any error condition which can indicate that a write or erase was in progress when the system was reset due to a voltage drop. If either the PRETRY or ERETRY bits are set, the peripheral should be reset by setting and then clearing the R0 bit in the EEPROM Software Reset (SREEPROM) register and waiting for the WORKING bit in the EEDONE register to clear before again checking the EESUPP register for error indicators. This procedure should allow the EEPROM to recover from the write or erase error. In very isolated cases, the EESUPP register can continue to register an error after this operation, in which case the reset should be repeated. After recovery, the application should rewrite the data which was being programmed when the initial failure occurred.