SLAU813A September 2019 – October 2020
Most of the register settings are done on the Device Monitor & Control window. The TPA6304-Q1 Register Map window is for reference.
Click the CONNECT button on the bottom left corner of the TPA6304Q1EVM application window, see Figure 3-6. The LED next to the TPA6304Q1EVM changes from gray to green and the CONNECT button changes to a DISCONNECT button.
Click on the TPA6304-Q1 Device Monitor & Control box, the window should now display Figure 4-2.
Figure 4-2 Device Monitor & Control WindowThis window has 8 major sections: the Device State Control section, Channel Control section, Miscellaneous Control section, Fault / Warning Signal Configuration section, Faults and Warnings section, AC Load Diagnostics section, DC Load Diagnostics section, and Spread Spectrum Controls section.