SLAU813A September 2019 – October 2020 TPA6304-Q1
This section allows the user to control all 4 channels at the same time instead of changing one channel at a time. When Hi-Z is selected, all 4 channels are put in Hi-Z. The display for each channel in the channel control section reflects these button selections.
To the right hand side of the Device State Control section is the Master/Slave Mode Selector switch. The default state of the device is Master Mode.