SLAU965 May 2025
The evaluation kit contains only the TAS5830EVM. A speaker is not included in the kit, but any speaker or dummy load rated for the expected output power can be connected to the output connectors. Similarly, a power supply is not a part of the kit and must be supplied to the appropriate banana jacks depending on if the Class-H algorithm or constant supply voltage is wanted. A micro-USB cable is also required if software mode is used.