SNAA434 March 2025 LMX2820
Figure 4-1 shows a general approach of combining multiple sources to drive a single load. The assumption is that all the sources are the same amplitude and output impedance and the output impedance of a single source is equal to the load.
The value of the matching resistor can be calculated as follows ( Appendix A ):
This matching is possible provided that:
For the purpose of analysis, a useful quantity to know the equivalent resistance of the load in parallel with N-1 sources.
From this the relative power can be calculated.
The isolation between source A and source B can be defined as the voltage that source A produces across the source impedance of source B. This can be expressed in dB.