The DS160PR4xx is highly programmable and customizable for multiple applications. The following sections provide guidance for programming the DS160PR4xx for common applications.
The following information is provided in each sequence:
- Step: Many sequences contain several steps. The order in which actions are to be taken is indicated by the step number.
- Register Set: Actions are intended for either the Shared or Channel register of either Bank 0 or Bank 1. Since each channel bank has its own I2CSMBus address, no explicit channel bank selection is necessary.
- Operation: Read or Write. If it is a Read operation, a register value or write mask is not associated.
- Register Address: Select the register to write to.
- Register Value: Value to write to register address.
- Write Mask: Unless the write mask is 0xFF, all writes should be performed as a read/modify/write operation. Only the bits identified by the mask should be modified.