SPRABV4I October   2021  – August 2025 SM320F28335-EP , SM320F28335-HT , TMS320F280023-Q1 , TMS320F280025-Q1 , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F2802-Q1 , TMS320F28020 , TMS320F280200 , TMS320F28021 , TMS320F28022 , TMS320F28022-Q1 , TMS320F280220 , TMS320F28023 , TMS320F28023-Q1 , TMS320F280230 , TMS320F28026 , TMS320F28026-Q1 , TMS320F28026F , TMS320F28027 , TMS320F28027-Q1 , TMS320F280270 , TMS320F28027F , TMS320F28027F-Q1 , TMS320F28030 , TMS320F28030-Q1 , TMS320F28031 , TMS320F28031-Q1 , TMS320F28032 , TMS320F28032-Q1 , TMS320F28033 , TMS320F28033-Q1 , TMS320F28034 , TMS320F28034-Q1 , TMS320F28035 , TMS320F28035-EP , TMS320F28035-Q1 , TMS320F28050 , TMS320F28051 , TMS320F28052 , TMS320F28052-Q1 , TMS320F28052F , TMS320F28052F-Q1 , TMS320F28052M , TMS320F28052M-Q1 , TMS320F28053 , TMS320F28054 , TMS320F28054-Q1 , TMS320F28054F , TMS320F28054F-Q1 , TMS320F28054M , TMS320F28054M-Q1 , TMS320F28055 , TMS320F2806-Q1 , TMS320F28062 , TMS320F28062-Q1 , TMS320F28062F , TMS320F28062F-Q1 , TMS320F28063 , TMS320F28064 , TMS320F28065 , TMS320F28066 , TMS320F28066-Q1 , TMS320F28067 , TMS320F28067-Q1 , TMS320F28068F , TMS320F28068M , TMS320F28069 , TMS320F28069-Q1 , TMS320F28069F , TMS320F28069F-Q1 , TMS320F28069M , TMS320F28069M-Q1 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28332 , TMS320F28333 , TMS320F28334 , TMS320F28335 , TMS320F28335-Q1 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Programming Fundamentals
  6. 3ROM Bootloader
  7. 4Flash Kernel A
    1. 4.1 Implementation
      1. 4.1.1 Application Load
  8. 5Flash Kernel B
    1. 5.1 Implementation
      1. 5.1.1 Packet Format
      2. 5.1.2 CPU1 Kernel Commands
      3. 5.1.3 CPU2 Kernel Commands
      4. 5.1.4 Packet Data
      5. 5.1.5 Status Codes
    2. 5.2 F2838x SCI Flash Kernels
      1. 5.2.1 CPU1-CPU2 Kernels
        1. 5.2.1.1 Kernel Commands
      2. 5.2.2 CPU1-CM Kernels
        1. 5.2.2.1 Kernel Commands
      3. 5.2.3 Using the Projects With SCI Bootloader
        1. 5.2.3.1 CPU1-CPU2
        2. 5.2.3.2 CPU1-CM
      4. 5.2.4 Using the Projects With Code Composer Studio (CCS) Software
        1. 5.2.4.1 CPU1-CPU2
        2. 5.2.4.2 CPU1-CM
    3. 5.3 F28P65x SCI Flash Kernel
      1. 5.3.1 CPU1 Kernel
        1. 5.3.1.1 Host-Kernel Communication: ControlCard
        2. 5.3.1.2 Host-Kernel Communication: LaunchPad Development Kit
        3. 5.3.1.3 Kernel Commands
      2. 5.3.2 Using the Projects With SCI Bootloader
        1. 5.3.2.1 CPU1
      3. 5.3.3 Using the Projects With CCS
        1. 5.3.3.1 CPU1
    4. 5.4 F28P55x SCI Flash Kernel
      1. 5.4.1 Implementation
        1. 5.4.1.1 Specifying the Flash Banks and Sectors of the Application
      2. 5.4.2 Kernel
      3. 5.4.3 Using the Project With SCI Bootloader
      4. 5.4.4 Using the Project with CCS
  9. 6Example Implementation
    1. 6.1 Device Setup
      1. 6.1.1 Flash Kernels
      2. 6.1.2 Hardware
    2. 6.2 Host Application: serial_flash_programmer
      1. 6.2.1 Overview
      2. 6.2.2 Building and Running serial_flash_programmer Using Visual Studio
      3. 6.2.3 Running serial_flash_programmer for F2806x (Flash Kernel A)
      4. 6.2.4 Running serial_flash_programmer for F2837xD (Flash Kernel B)
    3. 6.3 Host Application: Firmware Updates on F28004x With SCI Flash Kernel
      1. 6.3.1 Overview
      2. 6.3.2 Boot Pin Configurations
      3. 6.3.3 Using Three Boot Modes
      4. 6.3.4 Performing Live Firmware Updates
  10. 7Troubleshooting
    1. 7.1 General
    2. 7.2 SCI Boot
    3. 7.3 F2837x
      1. 7.3.1 F2837xS
      2. 7.3.2 F2837xD
      3. 7.3.3 F2837xD LaunchPad™
    4. 7.4 F28P65x
  11. 8References
  12. 9Revision History

CPU1-CM Kernels

The F2838x CPU1-CM kernel projects utilize the SCI Bootloader to download the CPU1 application image and a modified bootloader to download the CM application image. The CPU1 and CM kernel and application files are entered as parameters to the serial_flash_programmer utility, and the CPU1 kernel is downloaded once the host has completed the autobaud lock with the CPU1 SCI ROM Bootloader. Once the CPU1 kernel has been downloaded, normal kernel operations can start such as DFU, Erase, etc.

Once the CPU1 operations are completed, the CM kernel can be downloaded by selecting either "Run CPU1 Load CM" or "Reset CPU1 Load CM". CPU1 first writes the CM boot mode needed to download the kernel. After setting the boot mode for CM, CPU1 jumps to a copy function where the CPU1 takes in the CM kernel being sent through SCI from the host and copies the CM kernel over to a buffer in CPU1 to CM IPC Message RAM. Once the CM kernel has filled up the buffer, it signals CM which then copies over the contents of the buffer into the intended address in CM RAM. A copy function for the CM side that communicates with the CPU1 copy function is written into S0RAM during the CM boot sequence. This function was compiled using an ARM compiler and is stored as a const array in CPU1 to CM message RAM. The CPU1 and CM copy functions work together to copy over the CM kernel until all of it has been written. CPU1 then sends the CM kernel entry address to CM which then jumps to this address to start kernel execution. The user can then perform any desired CM commands.

CPU1 keeps control of the SCI peripheral and sends over the data CM needs for its kernel functions when requested by CM. The CM kernel can signal the CPU1 kernel that it needs a certain function executed, for example sciaGetWordData. CPU1 will get the result of executing the function and place it into Message RAM for CM to copy over and use for any of its commands.

CPU1 has 9 Options CM has 7 Options
1. DFU 1. DFU
2. Erase 2. Erase
3. Verify 3. Verify
4. Unlock Zone 1 4. Unlock Zone 1
5. Unlock Zone 2 5. Unlock Zone 2
6. Run 6. Run
7. Reset 7. Reset
8. Run CPU1 Load CM
9. Reset CPU1 Load CM