SPRACZ5 December 2021 TDA4VM
This is a bit more involved due to multiple clients sending requests to the device manager to enable a particular module.
It could be R5 SPL, A72 SPL, A72 U-boot, Linux and remote core firmware. A careful audit of where the modules are enabled should be done. When we are using PSDKLA we need to remove the device tree nodes both from U-boot DTS and Linux Kernel DTS.
A careful audit of device manager debug logs is necessary to see if a module is explicitly turned on by any of the software entity.
DM built in with debug enabled can be used to get debug logs to analyze