SPRAD67A december 2022 – july 2023 AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
The Hardware Design Guide for AM6442, AM6441, AM6422, AM6421, AM6412, AM6411, AM2434, AM2432 and AM2431 processors provides a starting point for the engineers designing with any of these processors. This hardware design guide provides an overview of the design flow, design efforts and highlights important design aspects that must be addressed. Note that this document does not contain all of the information needed to complete the board design. In many cases, it refers to the device-specific collaterals and various other user's guides as sources for specific information.
The hardware design guide (document) is organized in a sequential manner. It starts from decisions that must be made during the initial planning stages of the design, through the selection of key devices, electrical, and thermal requirements. For ensuring a successful design, issues discussed in each of the section should be resolved before moving to the next section.
These processors have capabilities to help board designers address safety requirements.
This hardware design guide is focused on non-safety applications.