SPRAD67A december 2022 – july 2023 AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
These family of processors includes wide variety of peripherals and processing capabilities, not all of which will be used in every design. Consequently, the requirements for different designs using the same device can vary widely depending on the target application. Designers must understand the requirements before determining the details of the design. In addition, the design may require additional circuitry to operate correctly in the target environment. Refer latest collaterals on TI.com like the device-specific Data Sheet, Errata, TRM and EVM User's guide for selecting the device and to determine the following: