SPRADL4 January 2025 F29H850TU , F29H859TU-Q1
The examples provided were tested with F29H859TU8. To properly test the example, the memory window and breakpoints need to be utilized within Code Composer Studio™. The following steps were followed to program and test the project:
Figure 5-2 Break Points
Figure 5-3 Write to
EEPROM
Figure 5-4 Read Data
Figure 5-5 Erase Full EEPROM
Unit
Figure 5-6 Write to
EEPROMThe preceding steps were used to test the Page Mode configuration. The 64-bit mode configuration can also be tested with the same procedure. To enable 64-bit mode, change the definition in the EEPROM_Config.h file by un-commenting the _64_BIT_MODE directive and commenting out the PAGE_MODE directive.