SPRUIN7C March 2020 – March 2024 TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1
The LIN protocol defines a message frame format, shown in Figure 24-12. Each frame includes one master header, one response, one in-frame response space, and inter-byte spaces. In-frame-response and inter-byte spaces can be 0.
There is no arbitration in the definition of the LIN protocol; therefore, multiple slave nodes responding to a header can be detected as an error.
The LIN bus is a single-channel wired-AND bus. The bus has a binary level: either dominant for a value of 0 or recessive for a value of 1.
Figure 24-12 LIN Protocol Message Frame
Format: Master Header and
Response