SPRUIN7C March 2020 – March 2024 TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1
Since error detection and correction logic is part of safety critical logic, safety applications can need to make sure that the logic is always working fine (during run time also). To enable this, a test mode is provided, in which a user can modify the data bits (without modifying the ECC/Parity bits) or ECC/Parity bits directly. Using this feature, an ECC/Parity error can be injected into data.
Table 3-14 and Table 3-15 show the bit mapping for the ECC/Parity bits when the bits are read in RAMTEST mode using the respective addresses.
| Data Bits Location in Read Data | Content (ECC Memory) |
|---|---|
| 6:0 | ECC Code for lower 16 bits of data |
| 7 | Not Used |
| 14:8 | ECC Code for upper 16 bits of data |
| 15 | Not Used |
| 22:16 | ECC Code for address |
| 31:23 | Not Used |
| Data Bits Location in Read Data | Content (Parity Memory) |
|---|---|
| 0 | Parity for lower 16 bits of data |
| 7:1 | Not Used |
| 8 | Parity for upper 16 bits of data |
| 15:9 | Not Used |
| 16 | Parity for address |
| 31:17 | Not Used |