SPRUIZ1B July 2023 – August 2024 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
Table 5-37 lists the memory-mapped registers for the DCSM_Z2_REGS registers. All register offset addresses not listed in Table 5-37 should be considered as reserved locations and the register contents should not be modified.
| Offset | Acronym | Register Name | Write Protection | Section |
|---|---|---|---|---|
| 0h | Z2_LINKPOINTER | Zone 2 Link Pointer | Go | |
| 2h | Z2_OTPSECLOCK | Zone 2 OTP Secure Lock | Go | |
| 6h | Z2_LINKPOINTERERR | Link Pointer Error | Go | |
| 8h | Z2_GPREG1 | Zone 2 General Purpose Register-1 | Go | |
| Ah | Z2_GPREG2 | Zone 2 General Purpose Register-2 | Go | |
| Ch | Z2_GPREG3 | Zone 2 General Purpose Register-3 | Go | |
| Eh | Z2_GPREG4 | Zone 2 General Purpose Register-4 | Go | |
| 10h | Z2_CSMKEY0 | Zone 2 CSM Key 0 | Go | |
| 12h | Z2_CSMKEY1 | Zone 2 CSM Key 1 | Go | |
| 14h | Z2_CSMKEY2 | Zone 2 CSM Key 2 | Go | |
| 16h | Z2_CSMKEY3 | Zone 2 CSM Key 3 | Go | |
| 18h | Z2_CR | Zone 2 CSM Control Register | Go | |
| 1Ah | Z2_GRABSECT1R | Zone 2 Grab Flash Status Register 1 | Go | |
| 1Ch | Z2_GRABSECT2R | Zone 2 Grab Flash Status Register 2 | Go | |
| 1Eh | Z2_GRABSECT3R | Zone 2 Grab Flash Status Register 3 | Go | |
| 20h | Z2_GRABRAM1R | Zone 2 Grab RAM Status Register 1 | Go | |
| 22h | Z2_GRABRAM2R | Zone 2 Grab RAM Status Register 2 | Go | |
| 26h | Z2_EXEONLYSECT1R | Zone 2 Execute Only Flash Status Register 1 | Go | |
| 28h | Z2_EXEONLYSECT2R | Zone 2 Execute Only Flash Status Register 2 | Go | |
| 2Ah | Z2_EXEONLYRAM1R | Zone 2 Execute Only RAM Status Register 1 | Go |
Complex bit access types are encoded to fit into small table cells. Table 5-38 shows the codes that are used for access types in this section.
| Access Type | Code | Description |
|---|---|---|
| Read Type | ||
| R | R | Read |
| R-0 | R -0 | Read Returns 0s |
| Write Type | ||
| W | W | Write |
| Reset or Default Value | ||
| -n | Value after reset or the default value | |
Z2_LINKPOINTER is shown in Figure 5-35 and described in Table 5-39.
Return to the Summary Table.
Zone 2 Link Pointer
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | LINKPOINTER | ||||||||||||||||||||||||||||||
| R-0003FFFFh | R-0h | ||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-14 | RESERVED | R | 0003FFFFh | Reserved |
| 13-0 | LINKPOINTER | R | 0h | This is resolved Link-Pointer value which is generated by looking at the three physical Link-Pointer values loaded from OTP Reset type: SYSRSn |
Z2_OTPSECLOCK is shown in Figure 5-36 and described in Table 5-40.
Return to the Summary Table.
Zone 2 OTP Secure Lock
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | CRCLOCK | ||||||
| R-0h | R-0h | ||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| PSWDLOCK | RESERVED | JTAGLOCK | |||||
| R-0h | R-0h | R-1h | |||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-12 | RESERVED | R | 0h | Reserved |
| 11-8 | CRCLOCK | R | 0h | Value in this field gets loaded from Z2_CRCLOCK[3:0] when a read is issued to address location of Z2_CRCLOCK in OTP. 1111 : VCU has ability to calculate CRC on secure memories. Other Value : VCU doesn't have ability to calculate CRC on secure memories. Reset type: XRSn |
| 7-4 | PSWDLOCK | R | 0h | Value in this field gets loaded from Z2_PSWDLOCK[3:0] when a read is issued to address location of Z1_PSWDLOCK in OTP. 1111 : CSM password locations in OTP are not protected and can be read from debugger as well as code running from anywhere. Other Value : CSM password locations in OTP are protected and can't be read without unlocking CSM of that zone. Reset type: XRSn |
| 3-1 | RESERVED | R | 0h | Reserved |
| 0 | JTAGLOCK | R | 1h | Reflects the state of the JTAGLOCK feature. 0 : JTAG is not locked 1 : JTAG is locked This bit is a copy of the Z1_OTPSECLOCK.JTAGLOCK bit. Reset type: PORESETn |
Z2_LINKPOINTERERR is shown in Figure 5-37 and described in Table 5-41.
Return to the Summary Table.
Link Pointer Error
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||||||||||
| R-0-0h | |||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | Z2_LINKPOINTERERR | ||||||||||||||
| R-0-0h | R-0h | ||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-14 | RESERVED | R-0 | 0h | Reserved |
| 13-0 | Z2_LINKPOINTERERR | R | 0h | These bits indicate errors during formation of the resolved Link-Pointer value after the three physical Link-Pointer values loaded of OTP in flash. 0 : No Error. Other : Error on bit positions which is set to 1. Reset type: SYSRSn |
Z2_GPREG1 is shown in Figure 5-38 and described in Table 5-42.
Return to the Summary Table.
Zone 2 General Purpose Register-1
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| GPREG1 | |||||||||||||||||||||||||||||||
| R-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | GPREG1 | R | 0h | This field gets loaded with the contents of Z2OTP_GPREG1 locations in Zone2 USER-OTP when a dummy read is issued to that address. Users can use this register to load any general purpose non-voliate content from USER-OTP of Zone2 Reset type: SYSRSn |
Z2_GPREG2 is shown in Figure 5-39 and described in Table 5-43.
Return to the Summary Table.
Zone 2 General Purpose Register-2
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| GPREG2 | |||||||||||||||||||||||||||||||
| R-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | GPREG2 | R | 0h | This field gets loaded with the contents of Z2OTP_GPREG2 locations in Zone2 USER-OTP when a dummy read is issued to that address. Users can use this register to load any general purpose non-voliate content from USER-OTP of Zone2 Reset type: SYSRSn |
Z2_GPREG3 is shown in Figure 5-40 and described in Table 5-44.
Return to the Summary Table.
Zone 2 General Purpose Register-3
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| GPREG3 | |||||||||||||||||||||||||||||||
| R-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | GPREG3 | R | 0h | This field gets loaded with the contents of Z2OTP_GPREG3 locations in Zone2 USER-OTP when a dummy read is issued to that address. Users can use this register to load any general purpose non-voliate content from USER-OTP of Zone2 Reset type: SYSRSn |
Z2_GPREG4 is shown in Figure 5-41 and described in Table 5-45.
Return to the Summary Table.
Zone 2 General Purpose Register-4
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| GPREG4 | |||||||||||||||||||||||||||||||
| R-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | GPREG4 | R | 0h | This field gets loaded with the contents of Z2OTP_GPREG4 locations in Zone2 USER-OTP when a dummy read is issued to that address. Users can use this register to load any general purpose non-voliate content from USER-OTP of Zone2 Reset type: SYSRSn |
Z2_CSMKEY0 is shown in Figure 5-42 and described in Table 5-46.
Return to the Summary Table.
Zone 2 CSM Key 0
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Z2_CSMKEY0 | |||||||||||||||||||||||||||||||
| R/W-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | Z2_CSMKEY0 | R/W | 0h | To unlock Zone2, user needs to write this regsiter with exact value as Z2_CSMPSWD0, programmed in OTP (zone gets unlock only if 128 bit password in OTP match with value written in four CSMKEY registers.) Reset type: SYSRSn |
Z2_CSMKEY1 is shown in Figure 5-43 and described in Table 5-47.
Return to the Summary Table.
Zone 2 CSM Key 1
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Z2_CSMKEY1 | |||||||||||||||||||||||||||||||
| R/W-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | Z2_CSMKEY1 | R/W | 0h | To unlock Zone2, user needs to write this regsiter with exact value as Z2_CSMPSWD1, programmed in OTP (zone gets unlock only if 128 bit password in OTP match with value written in four CSMKEY registers.) Reset type: SYSRSn |
Z2_CSMKEY2 is shown in Figure 5-44 and described in Table 5-48.
Return to the Summary Table.
Zone 2 CSM Key 2
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Z2_CSMKEY2 | |||||||||||||||||||||||||||||||
| R/W-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | Z2_CSMKEY2 | R/W | 0h | To unlock Zone2, user needs to write this regsiter with exact value as Z2_CSMPSWD2, programmed in OTP (zone gets unlock only if 128 bit password in OTP match with value written in four CSMKEY registers.) Reset type: SYSRSn |
Z2_CSMKEY3 is shown in Figure 5-45 and described in Table 5-49.
Return to the Summary Table.
Zone 2 CSM Key 3
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Z2_CSMKEY3 | |||||||||||||||||||||||||||||||
| R/W-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | Z2_CSMKEY3 | R/W | 0h | To unlock Zone2, user needs to write this regsiter with exact value as Z2_CSMPSWD3, programmed in OTP (zone gets unlock only if 128 bit password in OTP match with value written in four CSMKEY registers.) Reset type: SYSRSn |
Z2_CR is shown in Figure 5-46 and described in Table 5-50.
Return to the Summary Table.
Zone 2 CSM Control Register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| FORCESEC | RESERVED | ||||||
| R-0/W-0h | R-0h | ||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | RESERVED | UNSECURE | ALLONE | ALLZERO | RESERVED | ||
| R-0h | R-0h | R-0h | R-0h | R-1h | R-0h | ||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | |||
| R-0-0h | R-0h | R-0h | R-0h | R-0h | |||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31 | FORCESEC | R-0/W | 0h | A write of '1' to this bit clears the CSMKEYx registers. If writing to this bit after performing an update of the security passwords, it is advised to immediately perform a dummy load of the passwords by initiating a read of the passwords from their flash locations. Reset type: SYSRSn |
| 30-24 | RESERVED | R | 0h | Reserved |
| 23 | RESERVED | R | 0h | Reserved |
| 22 | RESERVED | R | 0h | Reserved |
| 21 | UNSECURE | R | 0h | Indiacates the state of Zone. 0 : Zone is in lock(secure) state. 1 : Zone is in unlock(unsecure) state. Reset type: SYSRSn |
| 20 | ALLONE | R | 0h | Indicates the state of CSM passwords. 0 : Zone CSM Passwords are not all ones. 1 : Zone CSM Passwords are all ones. Reset type: SYSRSn |
| 19 | ALLZERO | R | 1h | Indicates the state of CSM passowrds. 0 : CSM Passwords are not all zeros. 1 : CSM Passwords are all zero and device is permanently locked. Reset type: SYSRSn |
| 18-16 | RESERVED | R | 0h | Reserved |
| 15-4 | RESERVED | R-0 | 0h | Reserved |
| 3 | RESERVED | R | 0h | Reserved |
| 2 | RESERVED | R | 0h | Reserved |
| 1 | RESERVED | R | 0h | Reserved |
| 0 | RESERVED | R | 0h | Reserved |
Z2_GRABSECT1R is shown in Figure 5-47 and described in Table 5-51.
Return to the Summary Table.
Zone 2 Grab Flash Status Register 1
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| GRAB_B1_SECT127_96 | GRAB_B1_SECT95_64 | GRAB_B1_SECT63_32 | GRAB_B1_SECT31_4 | ||||
| R-0h | R-0h | R-0h | R-0h | ||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| GRAB_B1_SECT3 | GRAB_B1_SECT2 | GRAB_B1_SECT1 | GRAB_B1_SECT0 | ||||
| R-0h | R-0h | R-0h | R-0h | ||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| GRAB_B0_SECT127_96 | GRAB_B0_SECT95_64 | GRAB_B0_SECT63_32 | GRAB_B0_SECT31_4 | ||||
| R-0h | R-0h | R-0h | R-0h | ||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| GRAB_B0_SECT3 | GRAB_B0_SECT2 | GRAB_B0_SECT1 | GRAB_B0_SECT0 | ||||
| R-0h | R-0h | R-0h | R-0h | ||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-30 | GRAB_B1_SECT127_96 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT1 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 29-28 | GRAB_B1_SECT95_64 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT1 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 27-26 | GRAB_B1_SECT63_32 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT1 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 25-24 | GRAB_B1_SECT31_4 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT1 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 23-22 | GRAB_B1_SECT3 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT1 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 21-20 | GRAB_B1_SECT2 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT1 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 19-18 | GRAB_B1_SECT1 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT1 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 17-16 | GRAB_B1_SECT0 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT1 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 15-14 | GRAB_B0_SECT127_96 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT1 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 13-12 | GRAB_B0_SECT95_64 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT1 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 11-10 | GRAB_B0_SECT63_32 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT1 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 9-8 | GRAB_B0_SECT31_4 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT1 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 7-6 | GRAB_B0_SECT3 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT1 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 5-4 | GRAB_B0_SECT2 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT1 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 3-2 | GRAB_B0_SECT1 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT1 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 1-0 | GRAB_B0_SECT0 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT1 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
Z2_GRABSECT2R is shown in Figure 5-48 and described in Table 5-52.
Return to the Summary Table.
Zone 2 Grab Flash Status Register 2
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| GRAB_B3_SECT127_96 | GRAB_B3_SECT95_64 | GRAB_B3_SECT63_32 | GRAB_B3_SECT31_4 | ||||
| R-0h | R-0h | R-0h | R-0h | ||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| GRAB_B3_SECT3 | GRAB_B3_SECT2 | GRAB_B3_SECT1 | GRAB_B3_SECT0 | ||||
| R-0h | R-0h | R-0h | R-0h | ||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| GRAB_B2_SECT127_96 | GRAB_B2_SECT95_64 | GRAB_B2_SECT63_32 | GRAB_B2_SECT31_4 | ||||
| R-0h | R-0h | R-0h | R-0h | ||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| GRAB_B2_SECT3 | GRAB_B2_SECT2 | GRAB_B2_SECT1 | GRAB_B2_SECT0 | ||||
| R-0h | R-0h | R-0h | R-0h | ||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-30 | GRAB_B3_SECT127_96 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT2 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 29-28 | GRAB_B3_SECT95_64 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT2 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 27-26 | GRAB_B3_SECT63_32 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT2 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 25-24 | GRAB_B3_SECT31_4 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT2 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 23-22 | GRAB_B3_SECT3 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT2 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 21-20 | GRAB_B3_SECT2 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT2 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 19-18 | GRAB_B3_SECT1 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT2 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 17-16 | GRAB_B3_SECT0 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT2 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 15-14 | GRAB_B2_SECT127_96 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT2 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 13-12 | GRAB_B2_SECT95_64 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT2 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 11-10 | GRAB_B2_SECT63_32 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT2 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 9-8 | GRAB_B2_SECT31_4 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT2 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 7-6 | GRAB_B2_SECT3 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT2 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 5-4 | GRAB_B2_SECT2 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT2 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 3-2 | GRAB_B2_SECT1 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT2 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 1-0 | GRAB_B2_SECT0 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT2 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
Z2_GRABSECT3R is shown in Figure 5-49 and described in Table 5-53.
Return to the Summary Table.
Zone 2 Grab Flash Status Register 3
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| GRAB_B4_SECT127_96 | GRAB_B4_SECT95_64 | GRAB_B4_SECT63_32 | GRAB_B4_SECT31_4 | ||||
| R-0h | R-0h | R-0h | R-0h | ||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| GRAB_B4_SECT3 | GRAB_B4_SECT2 | GRAB_B4_SECT1 | GRAB_B4_SECT0 | ||||
| R-0h | R-0h | R-0h | R-0h | ||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-14 | GRAB_B4_SECT127_96 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT3 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 13-12 | GRAB_B4_SECT95_64 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT3 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 11-10 | GRAB_B4_SECT63_32 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT3 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 9-8 | GRAB_B4_SECT31_4 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT3 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 7-6 | GRAB_B4_SECT3 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT3 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 5-4 | GRAB_B4_SECT2 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT3 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 3-2 | GRAB_B4_SECT1 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT3 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 1-0 | GRAB_B4_SECT0 | R | 0h | Value in this field gets loaded from the equivalent bit field when a read is issued to the active ZSB address location of Z2_GRABSECT3 in the SECURITY sector. 00 : Invalid. Sectors are inaccessible. 01 : Request to allocate thes sectors to Zone2. 10 : No request for these sectors. 11 : No request for these sectors when this zone is UNLOCKED. Else these sectors are inaccessible if this zone is LOCKED. Reset type: SYSRSn |
Z2_GRABRAM1R is shown in Figure 5-50 and described in Table 5-54.
Return to the Summary Table.
Zone 2 Grab RAM Status Register 1
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| GRAB_RAM15 | GRAB_RAM14 | GRAB_RAM13 | GRAB_RAM12 | ||||
| R-0h | R-0h | R-0h | R-0h | ||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| GRAB_RAM11 | GRAB_RAM10 | GRAB_RAM9 | GRAB_RAM8 | ||||
| R-0h | R-0h | R-0h | R-0h | ||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| GRAB_RAM7 | GRAB_RAM6 | GRAB_RAM5 | GRAB_RAM4 | ||||
| R-0h | R-0h | R-0h | R-0h | ||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| GRAB_RAM3 | GRAB_RAM2 | GRAB_RAM1 | GRAB_RAM0 | ||||
| R-0h | R-0h | R-0h | R-0h | ||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-30 | GRAB_RAM15 | R | 0h | Value in this field gets loaded from Z2_GRABRAM1[31:30] when a read is issued to address location of Z2_GRABRAM1 in OTP. 00 : Invalid. D5 RAM is inaccessible. 01 : Request to allocate D5 RAM to Zone1. 10 : No request for D5 RAM 11 : No request for D5 RAM when this zone is UNLOCKED. Else D2 RAM is inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 29-28 | GRAB_RAM14 | R | 0h | Value in this field gets loaded from Z2_GRABRAM1[29:28] when a read is issued to address location of Z2_GRABRAM1 in OTP. 00 : Invalid. D4 RAM is inaccessible. 01 : Request to allocate D4 RAM to Zone1. 10 : No request for D4 RAM 11 : No request for D4 RAM when this zone is UNLOCKED. Else D2 RAM is inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 27-26 | GRAB_RAM13 | R | 0h | Value in this field gets loaded from Z2_GRABRAM1[27:26] when a read is issued to address location of Z2_GRABRAM1 in OTP. 00 : Invalid. D3 RAM is inaccessible. 01 : Request to allocate D3 RAM to Zone1. 10 : No request for D3 RAM 11 : No request for D3 RAM when this zone is UNLOCKED. Else D2 RAM is inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 25-24 | GRAB_RAM12 | R | 0h | Value in this field gets loaded from Z2_GRABRAM1[25:24] when a read is issued to address location of Z2_GRABRAM1 in OTP. 00 : Invalid. D2 RAM is inaccessible. 01 : Request to allocate D2 RAM to Zone2. 10 : No request for D2 RAM 11 : No request for D2 RAM when this zone is UNLOCKED. Else D2 RAM is inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 23-22 | GRAB_RAM11 | R | 0h | Value in this field gets loaded from Z2_GRABRAM1[23:22] when a read is issued to address location of Z2_GRABRAM1 in OTP. 00 : Invalid. D1 RAM is inaccessible. 01 : Request to allocate D1 RAM to Zone2. 10 : No request for D1 RAM 11 : No request for D1 RAM when this zone is UNLOCKED. Else D1 RAM is inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 21-20 | GRAB_RAM10 | R | 0h | Value in this field gets loaded from Z2_GRABRAM1[21:20] when a read is issued to address location of Z2_GRABRAM1 in OTP. 00 : Invalid. D0 RAM is inaccessible. 01 : Request to allocate D0 RAM to Zone2. 10 : No request for D0 RAM 11 : No request for D0 RAM when this zone is UNLOCKED. Else D0 RAM is inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 19-18 | GRAB_RAM9 | R | 0h | Value in this field gets loaded from Z2_GRABRAM1[19:18] when a read is issued to address location of Z2_GRABRAM1 in OTP. 00 : Invalid. CPU1 LS9 RAM is inaccessible. 01 : Request to allocate CPU1 LS9 RAM to Zone1. 10 : No request for CPU1 LS9 RAM 11 : No request for CPU1 LS9 RAM when this zone is UNLOCKED. Else CPU1 LS9 RAM is inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 17-16 | GRAB_RAM8 | R | 0h | Value in this field gets loaded from Z2_GRABRAM1[17:16] when a read is issued to address location of Z2_GRABRAM1 in OTP. 00 : Invalid. CPU1 LS8 RAM is inaccessible. 01 : Request to allocate CPU1 LS8 RAM to Zone1. 10 : No request for CPU1 LS8 RAM 11 : No request for CPU1 LS8 RAM when this zone is UNLOCKED. Else CPU1 LS8 RAM is inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 15-14 | GRAB_RAM7 | R | 0h | Value in this field gets loaded from Z2_GRABRAM1[15:14] when a read is issued to address location of Z2_GRABRAM1 in OTP. 00 : Invalid. CPU1 LS7 RAM is inaccessible. 01 : Request to allocate CPU1 LS7 RAM to Zone2. 10 : No request for CPU1 LS7 RAM 11 : No request for CPU1 LS7 RAM when this zone is UNLOCKED. Else CPU1 LS7 RAM is inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 13-12 | GRAB_RAM6 | R | 0h | Value in this field gets loaded from Z2_GRABRAM1[13:12] when a read is issued to address location of Z2_GRABRAM1 in OTP. 00 : Invalid. CPU1 LS6 RAM is inaccessible. 01 : Request to allocate CPU1 LS6 RAM to Zone2. 10 : No request for CPU1 LS6 RAM 11 : No request for CPU1 LS6 RAM when this zone is UNLOCKED. Else CPU1 LS6 RAM is inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 11-10 | GRAB_RAM5 | R | 0h | Value in this field gets loaded from Z2_GRABRAM1[11:10] when a read is issued to address location of Z2_GRABRAM1 in OTP. 00 : Invalid. CPU1 LS5 RAM is inaccessible. 01 : Request to allocate CPU1 LS5 RAM to Zone2. 10 : No request for CPU1 LS5 RAM 11 : No request for CPU1 LS5 RAM when this zone is UNLOCKED. Else CPU1 LS5 RAM is inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 9-8 | GRAB_RAM4 | R | 0h | Value in this field gets loaded from Z2_GRABRAM1[9:8] when a read is issued to address location of Z2_GRABRAM1 in OTP. 00 : Invalid. CPU1 LS4 RAM is inaccessible. 01 : Request to allocate CPU1 LS4 RAM to Zone2. 10 : No request for CPU1 LS4 RAM 11 : No request for CPU1 LS4 RAM when this zone is UNLOCKED. Else CPU1 LS4 RAM is inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 7-6 | GRAB_RAM3 | R | 0h | Value in this field gets loaded from Z2_GRABRAM1[7:6] when a read is issued to address location of Z2_GRABRAM1 in OTP. 00 : Invalid. CPU1 LS3 RAM is inaccessible. 01 : Request to allocate CPU1 LS3 RAM to Zone2. 10 : No request for CPU1 LS3 RAM 11 : No request for CPU1 LS3 RAM when this zone is UNLOCKED. Else CPU1 LS3 RAM is inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 5-4 | GRAB_RAM2 | R | 0h | Value in this field gets loaded from Z2_GRABRAM1[5:4] when a read is issued to address location of Z2_GRABRAM1 in OTP. 00 : Invalid. CPU1 LS2 RAM is inaccessible. 01 : Request to allocate CPU1 LS2 RAM to Zone2. 10 : No request for CPU1 LS2 RAM 11 : No request for CPU1 LS2 RAM when this zone is UNLOCKED. Else CPU1 LS2 RAM is inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 3-2 | GRAB_RAM1 | R | 0h | Value in this field gets loaded from Z2_GRABRAM1[3:2] when a read is issued to address location of Z2_GRABRAM1 in OTP. 00 : Invalid. CPU1 LS1 RAM is inaccessible. 01 : Request to allocate CPU1 LS1 RAM to Zone2. 10 : No request for CPU1 LS1 RAM 11 : No request for CPU1 LS1 RAM when this zone is UNLOCKED. Else CPU1 LS1 RAM is inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 1-0 | GRAB_RAM0 | R | 0h | Value in this field gets loaded from Z2_GRABRAM1[1:0] when a read is issued to address location of Z2_GRABRAM1 in OTP. 00 : Invalid. CPU1 LS0 RAM is inaccessible. 01 : Request to allocate CPU1 LS0 RAM to Zone2. 10 : No request for CPU1 LS0 RAM 11 : No request for CPU1 LS0 RAM when this zone is UNLOCKED. Else CPU1 LS0 RAM is inaccessible if this zone is LOCKED. Reset type: SYSRSn |
Z2_GRABRAM2R is shown in Figure 5-51 and described in Table 5-55.
Return to the Summary Table.
Zone 2 Grab RAM Status Register 2
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| GRAB_RAM15 | GRAB_RAM14 | GRAB_RAM13 | GRAB_RAM12 | ||||
| R-0h | R-0h | R-0h | R-0h | ||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-8 | RESERVED | R | 0h | Reserved |
| 7-6 | GRAB_RAM15 | R | 0h | Value in this field gets loaded from Z2_GRABRAM2[7:6] when a read is issued to address location of Z2_GRABRAM2 in OTP. Defines Zone2's grab request of the higher addressed half of CPU2TOCPU1MSGRAM0. 00 : Invalid. MSG RAM is inaccessible. 01 : Request to allocate MSG RAM to Zone2. 10 : No request for MSG RAM 11 : No request for MSG RAM when this zone is UNLOCKED. Else MSG RAM is inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 5-4 | GRAB_RAM14 | R | 0h | Value in this field gets loaded from Z2_GRABRAM2[5:4] when a read is issued to address location of Z2_GRABRAM2 in OTP. Defines Zone2's grab request of the lower addressed half of CPU2TOCPU1MSGRAM0. 00 : Invalid. MSG RAM is inaccessible. 01 : Request to allocate MSG RAM to Zone2. 10 : No request for MSG RAM 11 : No request for MSG RAM when this zone is UNLOCKED. Else MSG RAM is inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 3-2 | GRAB_RAM13 | R | 0h | Value in this field gets loaded from Z2_GRABRAM2[3:2] when a read is issued to address location of Z2_GRABRAM2 in OTP. Defines Zone2's grab request of the higher addressed half of CPU1TOCPU2MSGRAM0. 00 : Invalid. MSG RAM is inaccessible. 01 : Request to allocate MSG RAM to Zone2. 10 : No request for MSG RAM 11 : No request for MSG RAM when this zone is UNLOCKED. Else MSG RAM is inaccessible if this zone is LOCKED. Reset type: SYSRSn |
| 1-0 | GRAB_RAM12 | R | 0h | Value in this field gets loaded from Z2_GRABRAM2[1:0] when a read is issued to address location of Z2_GRABRAM2 in OTP. Defines Zone2's grab request of the lower addressed half of CPU1TOCPU2MSGRAM0. 00 : Invalid. MSG RAM is inaccessible. 01 : Request to allocate MSG RAM to Zone2. 10 : No request for MSG RAM 11 : No request for MSG RAM when this zone is UNLOCKED. Else MSG RAM is inaccessible if this zone is LOCKED. Reset type: SYSRSn |
Z2_EXEONLYSECT1R is shown in Figure 5-52 and described in Table 5-56.
Return to the Summary Table.
Zone 2 Execute Only Flash Status Register 1
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| EXEONLY_B3_SECT127_96 | EXEONLY_B3_SECT95_64 | EXEONLY_B3_SECT63_32 | EXEONLY_B3_SECT31_4 | EXEONLY_B3_SECT3 | EXEONLY_B3_SECT2 | EXEONLY_B3_SECT1 | EXEONLY_B3_SECT0 |
| R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| EXEONLY_B2_SECT127_96 | EXEONLY_B2_SECT95_64 | EXEONLY_B2_SECT63_32 | EXEONLY_B2_SECT31_4 | EXEONLY_B2_SECT3 | EXEONLY_B2_SECT2 | EXEONLY_B2_SECT1 | EXEONLY_B2_SECT0 |
| R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| EXEONLY_B1_SECT127_96 | EXEONLY_B1_SECT95_64 | EXEONLY_B1_SECT63_32 | EXEONLY_B1_SECT31_4 | EXEONLY_B1_SECT3 | EXEONLY_B1_SECT2 | EXEONLY_B1_SECT1 | EXEONLY_B1_SECT0 |
| R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| EXEONLY_B0_SECT127_96 | EXEONLY_B0_SECT95_64 | EXEONLY_B0_SECT63_32 | EXEONLY_B0_SECT31_4 | EXEONLY_B0_SECT3 | EXEONLY_B0_SECT2 | EXEONLY_B0_SECT1 | EXEONLY_B0_SECT0 |
| R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31 | EXEONLY_B3_SECT127_96 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
| 30 | EXEONLY_B3_SECT95_64 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
| 29 | EXEONLY_B3_SECT63_32 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
| 28 | EXEONLY_B3_SECT31_4 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
| 27 | EXEONLY_B3_SECT3 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
| 26 | EXEONLY_B3_SECT2 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
| 25 | EXEONLY_B3_SECT1 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
| 24 | EXEONLY_B3_SECT0 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
| 23 | EXEONLY_B2_SECT127_96 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
| 22 | EXEONLY_B2_SECT95_64 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
| 21 | EXEONLY_B2_SECT63_32 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
| 20 | EXEONLY_B2_SECT31_4 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
| 19 | EXEONLY_B2_SECT3 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
| 18 | EXEONLY_B2_SECT2 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
| 17 | EXEONLY_B2_SECT1 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
| 16 | EXEONLY_B2_SECT0 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
| 15 | EXEONLY_B1_SECT127_96 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
| 14 | EXEONLY_B1_SECT95_64 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
| 13 | EXEONLY_B1_SECT63_32 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
| 12 | EXEONLY_B1_SECT31_4 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
| 11 | EXEONLY_B1_SECT3 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
| 10 | EXEONLY_B1_SECT2 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
| 9 | EXEONLY_B1_SECT1 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
| 8 | EXEONLY_B1_SECT0 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
| 7 | EXEONLY_B0_SECT127_96 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
| 6 | EXEONLY_B0_SECT95_64 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
| 5 | EXEONLY_B0_SECT63_32 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
| 4 | EXEONLY_B0_SECT31_4 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
| 3 | EXEONLY_B0_SECT3 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
| 2 | EXEONLY_B0_SECT2 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
| 1 | EXEONLY_B0_SECT1 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
| 0 | EXEONLY_B0_SECT0 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT1 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for this sector (only if it is allocated to Zone2) 1 : Execute-Only protection is disabled for this sector (only if it is allocated to Zone2) Reset type: SYSRSn |
Z2_EXEONLYSECT2R is shown in Figure 5-53 and described in Table 5-57.
Return to the Summary Table.
Zone 2 Execute Only Flash Status Register 2
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| EXEONLY_B4_SECT127_96 | EXEONLY_B4_SECT95_64 | EXEONLY_B4_SECT63_32 | EXEONLY_B4_SECT31_4 | EXEONLY_B4_SECT3 | EXEONLY_B4_SECT2 | EXEONLY_B4_SECT1 | EXEONLY_B4_SECT0 |
| R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-8 | RESERVED | R | 0h | Reserved |
| 7 | EXEONLY_B4_SECT127_96 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT2 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for these sectors (only if they are allocated to Zone2) 1 : Execute-Only protection is disabled for these sectors (only if they are allocated to Zone2) Reset type: SYSRSn |
| 6 | EXEONLY_B4_SECT95_64 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT2 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for these sectors (only if they are allocated to Zone2) 1 : Execute-Only protection is disabled for these sectors (only if they are allocated to Zone2) Reset type: SYSRSn |
| 5 | EXEONLY_B4_SECT63_32 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT2 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for these sectors (only if they are allocated to Zone2) 1 : Execute-Only protection is disabled for these sectors (only if they are allocated to Zone2) Reset type: SYSRSn |
| 4 | EXEONLY_B4_SECT31_4 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT2 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for these sectors (only if they are allocated to Zone2) 1 : Execute-Only protection is disabled for these sectors (only if they are allocated to Zone2) Reset type: SYSRSn |
| 3 | EXEONLY_B4_SECT3 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT2 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for these sectors (only if they are allocated to Zone2) 1 : Execute-Only protection is disabled for these sectors (only if they are allocated to Zone2) Reset type: SYSRSn |
| 2 | EXEONLY_B4_SECT2 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT2 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for these sectors (only if they are allocated to Zone2) 1 : Execute-Only protection is disabled for these sectors (only if they are allocated to Zone2) Reset type: SYSRSn |
| 1 | EXEONLY_B4_SECT1 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT2 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for these sectors (only if they are allocated to Zone2) 1 : Execute-Only protection is disabled for these sectors (only if they are allocated to Zone2) Reset type: SYSRSn |
| 0 | EXEONLY_B4_SECT0 | R | 0h | Value in this bit gets loaded from the equivalent bit when a read is issued to the Z2_EXEONLYSECT2 address location in the SECURITY sector. 0 : Execute-Only protection is enabled for these sectors (only if they are allocated to Zone2) 1 : Execute-Only protection is disabled for these sectors (only if they are allocated to Zone2) Reset type: SYSRSn |
Z2_EXEONLYRAM1R is shown in Figure 5-54 and described in Table 5-58.
Return to the Summary Table.
Zone 2 Execute Only RAM Status Register 1
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| EXEONLY_RAM15 | EXEONLY_RAM14 | EXEONLY_RAM13 | EXEONLY_RAM12 | EXEONLY_RAM11 | EXEONLY_RAM10 | EXEONLY_RAM9 | EXEONLY_RAM8 |
| R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| EXEONLY_RAM7 | EXEONLY_RAM6 | EXEONLY_RAM5 | EXEONLY_RAM4 | EXEONLY_RAM3 | EXEONLY_RAM2 | EXEONLY_RAM1 | EXEONLY_RAM0 |
| R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15 | EXEONLY_RAM15 | R | 0h | Value in this field gets loaded from Z2_EXEONLYRAM1[15] when a read is issued to Z2_EXEONLYRAM address location in OTP. 0 : Execute-Only protection is enabled for D5 RAM (only if it's allocated to Zone2) 1 : Execute-Only protection is disabled for D5 RAM (only if it's allocated to Zone2) Reset type: SYSRSn |
| 14 | EXEONLY_RAM14 | R | 0h | Value in this field gets loaded from Z2_EXEONLYRAM1[14] when a read is issued to Z2_EXEONLYRAM address location in OTP. 0 : Execute-Only protection is enabled for D4 RAM (only if it's allocated to Zone2) 1 : Execute-Only protection is disabled for D4 RAM (only if it's allocated to Zone2) Reset type: SYSRSn |
| 13 | EXEONLY_RAM13 | R | 0h | Value in this field gets loaded from Z2_EXEONLYRAM1[13] when a read is issued to Z2_EXEONLYRAM address location in OTP. 0 : Execute-Only protection is enabled for D3 RAM (only if it's allocated to Zone2) 1 : Execute-Only protection is disabled for D3 RAM (only if it's allocated to Zone2) Reset type: SYSRSn |
| 12 | EXEONLY_RAM12 | R | 0h | Value in this field gets loaded from Z2_EXEONLYRAM1[12] when a read is issued to Z2_EXEONLYRAM address location in OTP. 0 : Execute-Only protection is enabled for D2 RAM (only if it's allocated to Zone2) 1 : Execute-Only protection is disabled for D2 RAM (only if it's allocated to Zone2) Reset type: SYSRSn |
| 11 | EXEONLY_RAM11 | R | 0h | Value in this field gets loaded from Z2_EXEONLYRAM1[11] when a read is issued to Z2_EXEONLYRAM address location in OTP. 0 : Execute-Only protection is enabled for D1 RAM (only if it's allocated to Zone2) 1 : Execute-Only protection is disabled for D1 RAM (only if it's allocated to Zone2) Reset type: SYSRSn |
| 10 | EXEONLY_RAM10 | R | 0h | Value in this field gets loaded from Z2_EXEONLYRAM1[10] when a read is issued to Z2_EXEONLYRAM address location in OTP. 0 : Execute-Only protection is enabled for D0 RAM (only if it's allocated to Zone2) 1 : Execute-Only protection is disabled for D0 RAM (only if it's allocated to Zone2) Reset type: SYSRSn |
| 9 | EXEONLY_RAM9 | R | 0h | Value in this field gets loaded from Z2_EXEONLYRAM1[9] when a read is issued to Z2_EXEONLYRAM address location in OTP. 0 : Execute-Only protection is enabled for CPU1 LS9 RAM (only if it's allocated to Zone2) 1 : Execute-Only protection is disabled for CPU1 LS9 RAM (only if it's allocated to Zone2) Reset type: SYSRSn |
| 8 | EXEONLY_RAM8 | R | 0h | Value in this field gets loaded from Z2_EXEONLYRAM1[8] when a read is issued to Z2_EXEONLYRAM address location in OTP. 0 : Execute-Only protection is enabled for CPU1 LS8 RAM (only if it's allocated to Zone2) 1 : Execute-Only protection is disabled for CPU1 LS8 RAM (only if it's allocated to Zone2) Reset type: SYSRSn |
| 7 | EXEONLY_RAM7 | R | 0h | Value in this field gets loaded from Z2_EXEONLYRAM1[7] when a read is issued to Z2_EXEONLYRAM address location in OTP. 0 : Execute-Only protection is enabled for CPU1 LS7 RAM (only if it's allocated to Zone2) 1 : Execute-Only protection is disabled for CPU1 LS7 RAM (only if it's allocated to Zone2) Reset type: SYSRSn |
| 6 | EXEONLY_RAM6 | R | 0h | Value in this field gets loaded from Z2_EXEONLYRAM1[6] when a read is issued to Z2_EXEONLYRAM1 address location in OTP. 0 : Execute-Only protection is enabled for CPU1 LS6 RAM (only if it's allocated to Zone2) 1 : Execute-Only protection is disabled for CPU1 LS6 RAM (only if it's allocated to Zone2) Reset type: SYSRSn |
| 5 | EXEONLY_RAM5 | R | 0h | Value in this field gets loaded from Z2_EXEONLYRAM1[5] when a read is issued to Z2_EXEONLYRAM1 address location in OTP. 0 : Execute-Only protection is enabled for CPU1 LS5 RAM (only if it's allocated to Zone2) 1 : Execute-Only protection is disabled for CPU1 LS5 RAM (only if it's allocated to Zone2) Reset type: SYSRSn |
| 4 | EXEONLY_RAM4 | R | 0h | Value in this field gets loaded from Z2_EXEONLYRAM1[4] when a read is issued to Z2_EXEONLYRAM1 address location in OTP. 0 : Execute-Only protection is enabled for CPU1 LS4 RAM (only if it's allocated to Zone2) 1 : Execute-Only protection is disabled for CPU1 LS4 RAM (only if it's allocated to Zone2) Reset type: SYSRSn |
| 3 | EXEONLY_RAM3 | R | 0h | Value in this field gets loaded from Z2_EXEONLYRAM1[3] when a read is issued to Z2_EXEONLYRAM1 address location in OTP. 0 : Execute-Only protection is enabled for CPU1 LS3 RAM (only if it's allocated to Zone2) 1 : Execute-Only protection is disabled for CPU1 LS3 RAM (only if it's allocated to Zone2) Reset type: SYSRSn |
| 2 | EXEONLY_RAM2 | R | 0h | Value in this field gets loaded from Z2_EXEONLYRAM1[2] when a read is issued to Z2_EXEONLYRAM1 address location in OTP. 0 : Execute-Only protection is enabled for CPU1 LS2 RAM (only if it's allocated to Zone2) 1 : Execute-Only protection is disabled for CPU1 LS2 RAM (only if it's allocated to Zone2) Reset type: SYSRSn |
| 1 | EXEONLY_RAM1 | R | 0h | Value in this field gets loaded from Z2_EXEONLYRAM1[1] when a read is issued to Z2_EXEONLYRAM1 address location in OTP. 0 : Execute-Only protection is enabled for CPU1 LS1 RAM (only if it's allocated to Zone2) 1 : Execute-Only protection is disabled for CPU1 LS1 RAM (only if it's allocated to Zone2) Reset type: SYSRSn |
| 0 | EXEONLY_RAM0 | R | 0h | Value in this field gets loaded from Z2_EXEONLYRAM1[0] when a read is issued to Z2_EXEONLYRAM1 address location in OTP. 0 : Execute-Only protection is enabled for CPU1 LS0 RAM (only if it's allocated to Zone2) 1 : Execute-Only protection is disabled for CPU1 LS0 RAM (only if it's allocated to Zone2) Reset type: SYSRSn |