This use-case demonstrates a scenario
for an application using three boot mode select pins to select between various boot
modes in the custom boot table.
- Program the BOOTPIN_CONFIG
location in OTP as follows:
- Set BOOTPIN_CONFIG.BMSP0
to a user specified GPIO, such as 0x0 for GPIO0
- Set BOOTPIN_CONFIG.BMSP1
to a user specified GPIO, such as 0x1 for GPIO1
- Set BOOTPIN_CONFIG.BMSP2
to a user specified GPIO, such as 0x2 for GPIO2
- Set BOOTPIN_CONFIG.KEY to
0x5A for boot ROM to treat these register bits as valid and use the
custom boot table.
- Program the BOOTDEF location
options for the device. This essentially sets up a device-specific boot mode
table. Refer to Section 4.7.9 for valid BOOTDEF values to set in the table.
- Set BOOTDEF.BOOTDEF0 to
0x02 for CAN booting. This sets CAN boot to boot table index 0.
- Set BOOTDEF.BOOTDEF1 to
0x03 for booting to Flash (entry address option 0). This sets Flash boot
to boot table index 1.
- Set BOOTDEF.BOOTDEF2 to
0x24 for booting to wait boot (alternate option). This sets wait boot to
boot table index 2.
- Set BOOTDEF.BOOTDEF3 to
0x66 for SPI booting (alternate GPIO option 3). This sets SPI boot to
boot table index 3.
- Set BOOTDEF.BOOTDEF4 to
0x43 for booting to Flash (entry address option 2). This sets Flash boot
to boot table index 4.
Table 4-14 Three Boot Pins Boot
Table Result
| Boot Mode Table Number |
Boot Mode |
| 0 |
CAN Boot (0x02) |
| 1 |
Flash Boot (0x03) |
| 2 |
Wait Boot - Alt (0x24) |
| 3 |
SPI - Alt3 (0x66) |
| 4 |
Flash Boot - Alt2 (0x43) |
| 5, 6, 7 |
Not used in this example |