SPRUJB6B November 2024 – May 2025 AM2612
| Trigger Input Bit | Source Signal | Comments |
|---|---|---|
| [7] | Reserved | |
| [6] | Reserved | |
| [5] | Reserved | |
| [4] | Reserved | |
| [3] | Reserved | |
| [2] | STM:ASYNCOUT | Alignment synchronization output. The STM asserts this signal for one clock cycle when an ASYNC-VERSION-FREQ sequence is output on the ATB interface, and the ASYNCOUT signal can be used for cross-triggering. |
| [1] | STM:TRIGOUTSW | The STM asserts this signal for one clock cycle when a trigger event is generated on writes to a TRIG location in the extended stimulus port registers |
| [0] | STM:TRIGOUTSPTE | The STM asserts this signal for one clock cycle when a trigger event is detected on a match using the STMSPTER. |