SPRUJB6B November 2024 – May 2025 AM2612
The TMU contains two operand registers: OP1 and OP2. The operand registers contain the input operand value for a TMU operation. One or two operand registers are used depending on which operation is being performed. The supported operations and number of operand registers are listed below. Further details can be found in Table 7-24.
The OP1 register does not need to maintain its input value for more than a CPU cycle due to the pipeline implementation of TMU operations. OP1 can also be overwritten in consecutive cycles with a new operand value for the same or different operation.