SPRUJB6B November 2024 – May 2025 AM2612
To avoid latency or processing delays between triggers, the application can write updated values to the NSEL, PHASE and SPREAD registers while the repeater module is still actively working. When a new SOC trigger is received, these values are loaded into the NCOUNT, PHASECOUNT and SPREADCOUNT registers, which then count down to zero as each SOC is triggered by the repeater module.
In addition, the application can change the repeater module's oversampling or undersampling mode by writing to the REPxCTL.MODE register while the repeater is actively working, without affecting the current operation. The repeater module loads the value of REPxCTL.MODE into REPxCTL.ACTIVEMODE when a new SOC trigger is received.