SPRUJF1C November   2024  – December 2025

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   5
  6. 1Evaluation Module Overview
    1. 1.1 Introduction
      1. 1.1.1 Preface: Read This First
        1. 1.1.1.1 Sitara MCU+ Academy
        2. 1.1.1.2 Important Usage Notes
    2. 1.2 Kit Contents
    3. 1.3 Device Information
      1. 1.3.1 System Architecture Overview
      2. 1.3.2 Component Identification
      3. 1.3.3 Functional Block Diagram
      4. 1.3.4 BoosterPacks
      5. 1.3.5 Device Information
        1. 1.3.5.1 Security
  7. 2Hardware
    1. 2.1  Setup
      1. 2.1.1 Standalone Configuration
    2. 2.2  Power Requirements
      1. 2.2.1 Power Input Using USB Type-C Connector
      2. 2.2.2 Power Tree
      3. 2.2.3 Power Status LEDs
    3. 2.3  Header Information
      1. 2.3.1 OSPI Expansion Connector
      2. 2.3.2 ADC/DAC External VREF Headers
      3. 2.3.3 FSI Header
      4. 2.3.4 EQEP Headers
    4. 2.4  Push Buttons
    5. 2.5  Reset
    6. 2.6  Clock
    7. 2.7  Boot Mode Selection
    8. 2.8  GPIO Mapping
    9. 2.9  IO Expander
    10. 2.10 Interfaces
      1. 2.10.1  Memory Interfaces
        1. 2.10.1.1 OSPI
        2. 2.10.1.2 Board ID EEPROM
      2. 2.10.2  Ethernet Interface
        1. 2.10.2.1 Ethernet PHY 0 - RGMII2 / PR0_PRU0
        2. 2.10.2.2 Ethernet PHY 1 - RGMII1 / PR0_PRU1
      3. 2.10.3  I2C
        1. 2.10.3.1 Industrial Application LEDs
      4. 2.10.4  SPI
      5. 2.10.5  UART
      6. 2.10.6  MCAN
      7. 2.10.7  SDFM
      8. 2.10.8  FSI
      9. 2.10.9  JTAG
      10. 2.10.10 Test Automation Pin Mapping
      11. 2.10.11 LIN
      12. 2.10.12 ADC and DAC
      13. 2.10.13 EQEP
      14. 2.10.14 EPWM
      15. 2.10.15 USB
    11. 2.11 BoosterPack Headers
      1. 2.11.1 BoosterPack Mode 00: Standard LaunchPad/BoosterPack Pinout
      2. 2.11.2 BoosterPack Mode 01: Servo Motor Control BoosterPacks Mode
      3. 2.11.3 BoosterPack Mode 10: BOOSTXL-IOLINKM-8 Mode
      4. 2.11.4 BoosterPack Mode 11: C2000 DRVx BoosterPacks Mode
    12. 2.12 Pinmux Mapping
    13. 2.13 Test Points
    14. 2.14 Best Practices
  8. 3Software
  9. 4Hardware Design Files
  10. 5Compliance
  11. 6Additional Information
    1. 6.1 Revision E1 Appendix
      1. 6.1.1 TA_POWERDOWNz pulled up by VSYS_TA_3V3 which is powered by VSYS_3V3
      2. 6.1.2 USB2.0_MUX_SEL0 pulled up by R355
      3. 6.1.3 MDIO and MDC of PRU0-ICSS0 needs to be routed to both Ethernet PHYs
      4. 6.1.4 AM261_RGMII1_RXLINK and AM261_RGMII2_RXLINK to be connected to GPIO
    2. 6.2 Revision E2 Appendix
      1. 6.2.1 Revision E2 Changes from E1
      2. 6.2.2 Revision E2 Known Limitations
    3. 6.3 Revision A Appendix
      1. 6.3.1 Revision A Changes from E2
      2. 6.3.2 Revision A Errata
    4.     Trademarks
  12. 7References
    1. 7.1 Reference Documents
    2. 7.2 Other TI Components Used in This Design
  13. 8Revision History

Boot Mode Selection

The boot mode for the AM261x is selected by a DIP (Dual In-Line Package) switch (SW4) or the test automation header. The test automation header uses an I2C expansion buffer to drive the boot mode when PORz is toggled. The supported boot modes are shown in Table 2-12. The DIP Switch configurations for each boot mode are shown in Table 2-13.

Note: The Boot Mode DIP Switch Positions on the LP-AM261 are the inverse of the SOPx settings. For example, if a boot mode setting calls for SOP3=0, then SW4.4=1.

LP-AM261 Boot mode DIP Switch Positions
                    - LP AM261x E2 SW1 SOP Switches

Figure 2-11 Boot mode DIP Switch Positions - LP AM261x E2 SW1 SOP Switches
Table 2-12 Supported Boot Modes
Boot Mode or Peripheral Boot Media or Host ROM Activity / Notes
OSPI-OSPI (4S), 50MHz, SDR, 0x6B Flash Memory ROM configures OSPI controller in OSPI 4S mode and downloads image from external flash, supports UART fallback boot mode if any failures
UART, XMODEM, 115200bps External Host ROM configures UART0 with baud rate of 115200 bps and downloads image from external PC terminal using x-modem protocol
OSPI-OSPI (1S), 50MHz, SDR, 0x0B Flash Memory ROM configures OSPI controller in OSPI 1S mode and downloads image from external flash, supports UART fallback boot mode if any failures
OSPI (8S), SDR, 33 MHz, 0x8B Flash Memory ROM configures OSPI controller in 8S mode and downloads image from external flash, supports UART fallback boot mode if any failures
DevBoot N/A To support SBL development, R5-will come up with ROM eclipsed, PLLs are initialized, No L2, TCMA and TCMB PBIST are performed, No L2 and TCM memInit. Supported only on FS devices
xSPI (1S->8D), 20 MHz, SFDP Flash Memory, External Host ROM configures OSPI controller in xSPI 8D mode, Reads SFDP table for read command and downloads image from external flash, Flashes with SFDP are of JEDEC standard Rev D only supported. In case of any failure it falls back to UART boot mode
USB DFU External Host ROM configures USB controller to work in device mode and download the image into L2 memory to process. In case of any failure it falls back to UART boot mode. Supports USB 2.0 device mode at High-Speed (HS, 480 Mbps)
Table 2-13 Boot Mode Selection
Boot Mode AM261x SOP[3:0] SW4.4 (SOP3 Inverse) SW4.3 (SOP2 Inverse) SW4.2 (SOP1 Inverse) SW4.1 (SOP0 Inverse)
OSPI-OSPI (4S), 50MHz, SDR, 0x6B 0000 1 1 1 1
UART, XMODEM, 115200bps 0001 1 1 1 0
OSPI-OSPI (1S), 50MHz, SDR, 0x0B 0010 1 1 0 1
OSPI (8S), SDR, 33 MHz, 0x8B 0011 1 1 0 0
DevBoot 1011 0 1 0 0
xSPI (1S->8D), 20 MHz, SFDP 1100 0 0 1 1
USB DFU 1110 0 0 0 1