SWRU368C May 2018 – January 2021 CC3100 , CC3100MOD , CC3200 , CC3200MOD
Functions used to set or get the domain name (used for accessing the web server in AP mode).
Function name | Description | Parameters |
---|---|---|
| Sets the domain name. Domain name format is string. | appId = SL_NET_APP_DEVICE_CONFIG_ID Option = NETAPP_SET_GET_DEV_CONF_OPT_DOMAIN_NAME OptionLen = domain name length pOptionValue = pointer to domain name |
| Gets current domain name. Domain name format is string (not null terminated). | appId = SL_NET_APP_DEVICE_CONFIG_ID Option = NETAPP_SET_GET_DEV_CONF_OPT_DOMAIN_NAME pOptionLen = user-supplied pointer for the returned domain name len pOptionValue = user-supplied pointer for the returned domain name |