SWRU368C May 2018 – January 2021 CC3100 , CC3100MOD , CC3200 , CC3200MOD
This section describes the P2P connection events. These events are sent by the device during connection and the user decides how to handle them.
SL_WLAN_P2P_NEG_REQ_RECEIVED_EVENT – This event is sent if the negotiation is ended successfully.
It contains:
SL_WLAN_CONNECTION_FAILED_EVENT – This event is sent if the connection fails, with the failure reason.
It contains:
SL_WLAN_CONNECT_EVENT – This event is shared by P2P client and station. Indicates that the P2P connection has ended successfully and that the device is a P2P client.
It contains:
SL_WLAN_CONNECT_EVENT – This event is shared for P2P GO and AP. Indicates that the P2P connection has ended successfully and that the device is P2P GO.
It contains: