SWRU543B January 2019 – June 2025 CC3230S , CC3230SF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
The flash memory controller can generate interrupts when one of the following conditions is observed:
The interrupt events that can trigger a controller-level interrupt are defined in the Flash Controller Masked Interrupt Status (FCMIS) register, by setting the corresponding MASK bits. If interrupts are not used, the raw interrupt status is always visible through the Flash Controller Raw Interrupt Status (FCRIS) register.
Interrupts are always cleared (for both the FCMIS and FCRIS registers) by writing 1 to the corresponding bit in the Flash Controller Masked Interrupt Status and Clear (FCMISC) register.