DLPU101E December   2020  – October 2025

 

  1.   1
  2.   Read This First
  3.   About This Guide
  4.   Trademarks
  5.   5
  6.   Related Documentation from Texas Instruments
  7.   If You Need Assistance
  8. 1DLP LightCrafter Single DLPC900 EVM Overview
    1. 1.1 Welcome
    2. 1.2 DLP LightCrafter Single DLPC900 Evaluation Module (EVM) Hardware
    3. 1.3 EVM Board
    4. 1.4 Other Items Needed for Operation
    5. 1.5 DLP LightCrafter Single DLPC900 Connections
      1. 1.5.1 DLP LightCrafter Single DLPC900 LED Enable and PWM Outputs
      2. 1.5.2 DLP LightCrafter Single DLPC900 Trigger Input and Output Voltage Selectors
    6. 1.6 DLP LightCrafter Single DLPC900 EVM Flex Cable
    7. 1.7 DLP LightCrafter Single DLPC900 EVM and DMD EVM Assembly
  9. 2Quick Start
    1. 2.1 Power-up the DLP LightCrafter Single DLPC900 EVM
    2. 2.2 Creating a Simple Pattern Sequence
  10. 3Operating the DLP LightCrafter Single DLPC900 EVM
    1. 3.1  DLP LightCrafter Single DLPC900 Control Software
    2. 3.2  PC Software
    3. 3.3  System Common Controls
      1. 3.3.1 Operating Mode
      2. 3.3.2 Connected DMD Type
      3. 3.3.3 EVM Information
      4. 3.3.4 Status
    4. 3.4  System Settings
    5. 3.5  Video Mode
      1. 3.5.1 Video Support
    6. 3.6  Pattern Modes
      1. 3.6.1 Menu Bar
      2. 3.6.2 Creating a Pattern Sequence in Pattern On-The-Fly Mode
      3. 3.6.3 Creating a Pattern Sequence in Pre-Stored Pattern Mode
      4. 3.6.4 Reordering a Pattern Sequence using the Edit LUT Feature
        1. 3.6.4.1 Special Considerations for Input Triggers when using the Edit LUT Feature
      5. 3.6.5 Creating a Pattern Sequence in Video Pattern Mode
      6. 3.6.6 Creating a Pattern Sequence With DMD Block Load
      7. 3.6.7 Pattern Settings
    7. 3.7  Batch Files
      1. 3.7.1 Execute Batch File
      2. 3.7.2 Creating and Saving Batch Files
        1. 3.7.2.1 Creating and Saving a Batch File Using the GUI
        2. 3.7.2.2 Creating a Batch File Using a Text Editor
      3. 3.7.3 Loading a Batch File
      4. 3.7.4 Adding a Batch File to the Firmware
    8. 3.8  Peripherals
      1. 3.8.1 Peripherals Tab
      2. 3.8.2 Debug Tab
    9. 3.9  Firmware
      1. 3.9.1 Adding or Removing Patterns from the Firmware
        1. 3.9.1.1 Deleting Images
        2. 3.9.1.2 Adding Images
        3. 3.9.1.3 Adding Both Images and Batch Files
      2. 3.9.2 Reprogram Firmware for a Different Supported DMD
    10. 3.10 Flash Device Parameters
    11. 3.11 JTAG Flash Programming
    12. 3.12 Programming an EDID
  11. 4Connectors
    1. 4.1  Input Trigger Connectors
    2. 4.2  Output Trigger Connectors
    3. 4.3  DLPC900 UART
    4. 4.4  DLPC900 I2C Port 0
    5. 4.5  DLPC900 I2C Port 1
    6. 4.6  DLPC900 I2C Port 2
    7. 4.7  JTAG Boundary Scan
    8. 4.8  GPIO and PWM
    9. 4.9  Power
    10. 4.10 External Parallel Video Connector
  12. 5Power Supply Requirements
    1. 5.1 External Power Supply Requirements
  13. 6Safety
    1. 6.1 Caution Labels
  14. 7Revision History

DLP LightCrafter Single DLPC900 Control Software

The DLPC900REF-SW bundle includes a GUI application to control the modules through the USB interface. QT is a cross-platform application and user-interface framework with open source and commercial licenses available. Install the QT-based GUI download and execute the latest DLPC900REF-SW Windows-Installer, and then start the DLP LightCrafter DLPC900 GUI application.

The following items are found in DLPC900REF-SW:

  • DLPC900REF-GUI – The software bundle includes the executable files for the PC-based Graphical User Interface (GUI) for easy communication over USB with the DLPC900 controller. The GUI was developed using the QT Library and QT Creator. The GUI source code is provided so that the user can customize as required or use as a reference to create a DLPC900 controller software interface.
  • DLPC900REF-JTAG – The JTAG Flash Programmer gives developers the ability to load the DLPR900 configuration firmware into flash memory attached to a DLPC900 controller. JTAG boundary scan programming allows developers to install the DLPR900 firmware in the absence of standard USB connectivity. For example, the JTAG Flash Programmer is used if the bootloader becomes corrupted and the board is rendered inoperable.
  • DLPC900REF-EDID – EDID files which can be programmed to the DLPLCRC900EVM or DLPLCRC900DEVM board according to the DMD the DLPC900 is controlling.
  • DLP9000-C900REF-FPGA – This binary file is used to configure the FPGA on the DLPLCRC900DEVM, to enable the display of 24-bit RGB data with dual DLPC900 controllers.

The DLP LightCrafter Single DLPC900 EVM supports two basic types of operation:

  • Video Mode displays images from:
    • HDMI and DisplayPort inputs.
    • 24-bit RGB customer provided bitmaps stored in flash memory.
    • Internal test pattern generator with ten user-selectable patterns.
    • Solid Full-screen Curtain with user-selectable colors.
  • Pattern Sequence displays images from:
    • Pre-stored Pattern Mode: 1-, 2-, 3-, 4-, 5-, 6-, 7-, and 8-bit user-defined bitmap images pre-stored in Flash memory.
    • Video Pattern Mode: 1-, 2-, 3-, 4-, 5-, 6-, 7-, and 8-bit user-define bitmap images streamed through the DLPC900 24-bit RGB interface.
    • Pattern On-the-Fly Mode: 1-, 2-, 3-, 4-, 5-, 6-, 7-, and 8-bit user-define bitmap images dynamically loaded into internal memory via USB or I2C interfaces.