DLPU101E December   2020  – October 2025

 

  1.   1
  2.   Read This First
  3.   About This Guide
  4.   Trademarks
  5.   5
  6.   Related Documentation from Texas Instruments
  7.   If You Need Assistance
  8. 1DLP LightCrafter Single DLPC900 EVM Overview
    1. 1.1 Welcome
    2. 1.2 DLP LightCrafter Single DLPC900 Evaluation Module (EVM) Hardware
    3. 1.3 EVM Board
    4. 1.4 Other Items Needed for Operation
    5. 1.5 DLP LightCrafter Single DLPC900 Connections
      1. 1.5.1 DLP LightCrafter Single DLPC900 LED Enable and PWM Outputs
      2. 1.5.2 DLP LightCrafter Single DLPC900 Trigger Input and Output Voltage Selectors
    6. 1.6 DLP LightCrafter Single DLPC900 EVM Flex Cable
    7. 1.7 DLP LightCrafter Single DLPC900 EVM and DMD EVM Assembly
  9. 2Quick Start
    1. 2.1 Power-up the DLP LightCrafter Single DLPC900 EVM
    2. 2.2 Creating a Simple Pattern Sequence
  10. 3Operating the DLP LightCrafter Single DLPC900 EVM
    1. 3.1  DLP LightCrafter Single DLPC900 Control Software
    2. 3.2  PC Software
    3. 3.3  System Common Controls
      1. 3.3.1 Operating Mode
      2. 3.3.2 Connected DMD Type
      3. 3.3.3 EVM Information
      4. 3.3.4 Status
    4. 3.4  System Settings
    5. 3.5  Video Mode
      1. 3.5.1 Video Support
    6. 3.6  Pattern Modes
      1. 3.6.1 Menu Bar
      2. 3.6.2 Creating a Pattern Sequence in Pattern On-The-Fly Mode
      3. 3.6.3 Creating a Pattern Sequence in Pre-Stored Pattern Mode
      4. 3.6.4 Reordering a Pattern Sequence using the Edit LUT Feature
        1. 3.6.4.1 Special Considerations for Input Triggers when using the Edit LUT Feature
      5. 3.6.5 Creating a Pattern Sequence in Video Pattern Mode
      6. 3.6.6 Creating a Pattern Sequence With DMD Block Load
      7. 3.6.7 Pattern Settings
    7. 3.7  Batch Files
      1. 3.7.1 Execute Batch File
      2. 3.7.2 Creating and Saving Batch Files
        1. 3.7.2.1 Creating and Saving a Batch File Using the GUI
        2. 3.7.2.2 Creating a Batch File Using a Text Editor
      3. 3.7.3 Loading a Batch File
      4. 3.7.4 Adding a Batch File to the Firmware
    8. 3.8  Peripherals
      1. 3.8.1 Peripherals Tab
      2. 3.8.2 Debug Tab
    9. 3.9  Firmware
      1. 3.9.1 Adding or Removing Patterns from the Firmware
        1. 3.9.1.1 Deleting Images
        2. 3.9.1.2 Adding Images
        3. 3.9.1.3 Adding Both Images and Batch Files
      2. 3.9.2 Reprogram Firmware for a Different Supported DMD
    10. 3.10 Flash Device Parameters
    11. 3.11 JTAG Flash Programming
    12. 3.12 Programming an EDID
  11. 4Connectors
    1. 4.1  Input Trigger Connectors
    2. 4.2  Output Trigger Connectors
    3. 4.3  DLPC900 UART
    4. 4.4  DLPC900 I2C Port 0
    5. 4.5  DLPC900 I2C Port 1
    6. 4.6  DLPC900 I2C Port 2
    7. 4.7  JTAG Boundary Scan
    8. 4.8  GPIO and PWM
    9. 4.9  Power
    10. 4.10 External Parallel Video Connector
  12. 5Power Supply Requirements
    1. 5.1 External Power Supply Requirements
  13. 6Safety
    1. 6.1 Caution Labels
  14. 7Revision History

Status

The Status panel indicators show the current state of the DLPC900. When any of the boxes are checked, this indicates the stated text has occurred. Any boxes that state an error and remain checked must be corrected before continuing to operate the EVM.

The following is a description of each status indicator:

  • Internal Memory Test Passed – The DLPC900 performs an internal system memory test at power-up. The box is checked if the test passed.
  • Controller/DMD Incompatible – The box is checked if either the controller or DMD are incompatible with the firmware including loading incorrect firmware or an issue with communication between the controller and DMD. Check for possible damage to the DMD SCP lines, or damage to the flex cable. Also verify that the DMD is sitting properly in the socket, and is not missing or damaged.
  • Secondary Present and Ready – The box is checked when the GUI is connected to a DLP LightCrafter Dual DLPC900 EVM. If the GUI is connected to a DLP LightCrafter Single DLPC900 EVM and the box is checked then the DLPC900 is potentially malfunctioning or was incorrectly programmed with one of the Dual DLPC900 firmware files.
  • Internal Initialization Complete – The box is checked when all power-up initialization routines have completed and passed.
  • DMD Reset Waveform Controller Error – The box is checked whenever the DMD Reset Controller has found multiple overlapping Vbias or reset operations accessing the same DMD block of micromirrors.
  • Forced Buffer Swap – The box is checked whenever a forced buffer swap occurs. This error can occur if the DLP LightCrafter Single DLPC900 EVM is set to Video Mode and the vertical back-porch timing is too small. The error can also occur if the DLP LightCrafter Single DLPC900 EVM is set to Video Pattern Mode where the patterns are from the video port and the pattern sequence timings do not match the video port VSYNC - specifically the cumulative exposure times are greater than the frame time. Forced buffer swaps can also occur during any of the pattern modes in preparing a pattern sequence and the timing of a status read. There is a possibility that the user needs to perform additional reads of the status to get a correct state of this indicator. If the box continues to be checked, then check for an error condition in the pattern sequence.
  • Sequence Abort Status Flag – The box is checked whenever a sequence abort has occurred. Sequence abort can occur during any pattern mode in preparing a pattern sequence and the timing of reading the status. Additional status reads can be needed to get a correct state of this indicator. If the box continues to be checked, then check for an error condition in the pattern sequence. Also check that the cumulative exposure time is not greater that the frame time.
  • Sequence Error – The box is checked whenever a sequence error has occurred. Sequence errors can occur during any of the pattern modes in preparing a pattern sequence and the timing of reading the status. The user can need to perform additional reads of the status to get a correct state of this indicator. If the box continues to be checked, then check for an error condition in the pattern sequence.
  • DMD Micromirrors Parked – The box is checked whenever the DMD micromirrors are parked.
  • Sequencer Running – The box is checked whenever the sequencer is running.
  • Video Running – The box is checked whenever video is running.
  • Locked to External Source – The box is checked to indicate that the EVM has locked to an external parallel RGB video source. If the EVM loses the locked signal at any time, the box becomes unchecked. A locked source must be present to switch to Video Pattern Mode.
  • DLPA200 Fault – The box is checked whenever a DLPA200 fault has occurred. The box is active when a DLP5500 DMD is connected.

  • DMD Communication error – The box is checked if the controller is unable communicate with the attached DMD.